2.2 Use of Double Pulse Generation Circuit
The ASD2-EVAL-001 Evaluation Board is provided with a double pulse generation circuit, as shown in the following figure. It consists of a switch (SW1) and three preset multi-turn potentiometers. By pressing switch SW1 once, a double pulse waveform is generated. Connect an external switch at connector J11 to generate a double-pulse waveform. POT R85 is used to set/change the pulse width of the first pulse, POT R96 is used to set/change the delay between the first and second pulse, and POT R97 is used to set/change the pulse width of the second pulse.
To characterize the High-Side device, place the jumper on pin 2 and pin 3 of the connector J9, and to characterize the Low‑Side device, place the jumper on pin 2 and pin 3 of the connector J10. In double pulse mode, only one device must be characterized at a time.