27.2.1 Starting a Conversion
To enable the ADC module, the ON bit must be set to ‘1’. A conversion may be started by
either of the following:
- Software setting the GO bit to ‘
1’ - An external trigger (source selected by the ADC Auto-Conversion Trigger (ADACT) register)
Important: The GO bit must
not be set in the same instruction that turns on the ADC. Refer to ADC Conversion Procedure for more
details.