3.10.2 mcKeyI_ValidationKeyGet
C
/* Get algorithms key */ char * mcKeyI_ValidationKeyGet( const tmcKey_IPs_s ip)
Summary
Get the algorithms key.
Description
This function is used to read the validation key for a specified IP (Intellectual
Property) from the global key data structure
mcKeyI_AlgorithmKeys_gds.
Precondition
None.
Parameters
| Param | Description |
|---|---|
| ip | Index value for accessing the
corresponding validation key in the Keys
array. |
Returns
Returns a pointer to the validation key corresponding to the specified IP from the
Keys array .
Example
tmcKey_IPs_s ip = KEY_IPD; // Example IP identifier
char *key = mcKeyI_ValidationKeyGet(ip);
Remarks
None.