12.5 Watchdog Timer
If the watchdog timer is not needed in the application, the module should be turned off. If the watchdog timer is enabled, it will be enabled in all sleep modes and hence always consume power. In the deeper sleep modes, this will contribute significantly to the total current consumption.
Refer to Watchdog System Reset for details on how to configure the watchdog timer.