24.4.3 Far Objects and Functions
The __far qualifier can be used to indicate that
variables or functions are located in ‘far memory’. Exactly what constitutes far memory is
dependent on the target device, but it is typically memory that requires more complex code
to access. Expressions involving far-qualified objects usually generate slower and larger
code.
Use the native keywords discussed in the Differences section to look up information on the semantics of this qualifier.
Some devices may not have such memory implemented, in which case, use of
this qualifier is ignored. Stack-based (auto and parameter) variables
cannot use the __far specifier.
Example
The following shows a variable and function qualified using
__far.
__far int serialNo;
__far int ext_getCond(int selector);
Differences
The 8-bit compilers have used the qualifier far to indicate this meaning.
Functions could not be qualified as far.
The 16-bit compilers have used the far attribute with both variables and
functions.
The 32-bit compilers have used the far attribute with functions only.
Migration to the CCI
For 8-bit compilers, change any occurrence of the far qualifier, e.g., from:
far char template[20];
to:
__far, i.e., __far char template[20];
In the 16- and 32-bit compilers, change any occurrence of the
far attribute, for example, from:
void bar(void) __attribute__ ((far));
int tblIdx __attribute__ ((far));
to:
void __far bar(void);
int __far tblIdx;
Caveats
None.