24.4.2 Absolute Addressing
Variables and functions can be placed at an absolute address by using the
__at() construct. Stack-based (auto and parameter)
variables cannot use the __at() specifier.
Example
The following shows two variables and a function being made absolute.
int scanMode __at(0x200);
const char keys[] __at(124) = { ’r’, ’s’, ’u’, ’d’};
__at(0x1000) int modify(int x) {
return x * 2 + 3;
}
Differences
The 8-bit compilers have used an @ symbol to specify an
absolute address. The 16- and 32-bit compilers have used the address
attribute to specify an object’s address.
Migration to the CCI
Avoid making objects and functions absolute if possible.
In MPLAB XC8, change absolute object definitions, e.g., from:
int scanMode @ 0x200;
to:
int scanMode __at(0x200);
In MPLAB XC16 and XC32, change code, for example, from:
int scanMode __attribute__((address(0x200)));
to:
int scanMode __at(0x200);
Caveats
If the __at() and __section() specifiers are both applied
to an object when using MPLAB XC8, the __section() specifier is currently
ignored.
The __at() specifier must be placed at the beginning of function
prototypes for the 16- and 32-bit compilers. If you prefer to use the specifier at the end
of the prototype, use the specifier with a declaration and leave it off the definition, for
example:
int modify(int x) __at(0x1000);
int modify(int x)
{ ... }