24.4.8 Alignment of Objects
The __align(alignment) specifier can be used to
indicate that variables must be aligned on a memory address that is a multiple of the
alignment specified. The alignment term must be a power of 2. Positive values request that
the object’s start address be aligned.
Example
The following shows variables qualified using __align()
to ensure they end on an address that is a multiple of 8, and start on an address that is a
multiple of 2, respectively.
__align(-8) int spacer;
__align(2) char coeffs[6];
Differences
An alignment feature has never been implemented on 8-bit compilers.
The 16- and 32-bit compilers used the aligned attribute with
variables.
Migration to the CCI
For 16- and 32-bit compilers, change any occurrence of the aligned
attribute to __aligned, for example, from:
char __attribute__((aligned(4)))mode;
to:
__align(4) char mode;