24.4.12 Indicating Antiquated Objects
The __deprecate specifier can be used to indicate that an
object has limited longevity and should not be used in new designs. It is commonly used by
the compiler vendor to indicate that compiler extensions or features can become obsolete,
or that better features have been developed and should be used in preference.
Use the native keywords discussed in the Differences section to look up information on the semantics of this specifier.
Example
The following shows a function that uses the __deprecate
keyword.
void __deprecate getValue(int mode)
{
//...
}
Differences
No deprecate feature was implemented on 8-bit compilers.
The 16-bit and 32-bit compilers have used the deprecated
attribute (note the different spelling) to indicate that objects should be avoided, if
possible.
Migration to the CCI
For 16- and 32-bit compilers, change any occurrence of the
deprecated attribute to __deprecate, for example,
from:
int __attribute__(deprecated) intMask;
to:
int __deprecate intMask;
Caveats
None.