5.6.4.3 Fill Flash Memory
| Option | Description | Command Line1 |
|---|---|---|
| Which areas to fill | Specify which area of Flash memory to fill. No Fill - None (default). Fill All Unused - Fill all unused memory. Provide Range to fill - Fill a range of memory. Enter a range under “Memory Address Range.” |
|
| How to fill it | Specify how to fill Flash memory. Provide sequence of values - provide a sequence under the Sequence option. Constant or incrementing value - provide a constant, increment/decrement or increment/decrement constant under the same-named option. | --fill=sequence |
| Sequence | When Provide sequence of values is selected, enter a sequence. The form is n1, n2, .... where n1 uses C syntax. Example: 0x10, 25, 0x3F, 16. | --fill=sequence |
| Constant | When Constant or incrementing value is selected, enter a constant. Specify the constant using C syntax (for example, 0x for hex, 0 for octal). Example: 0x10 is the same as 020 or 16. | --fill=sequence |
| Increment/Decrement | When Constant or incrementing value is selected, you can
select to increment or decrement the initial value of “Constant” on each
consecutive address. No Incrementing - do not change constant value. Increment Const - increment the constant value by the amount specified under the option “Increment/Decrement Constant.” Decrement Const - decrement the constant value by the amount specified under the option “Increment/Decrement Constant.” | --fill=sequence |
| Increment/Decrement Constant | When Increment Const or Decrement Const is selected, enter a constant increment or decrement value. Specify the constant using C syntax (for example, 0x for hex, 0 for octal). Example: 0x10 is the same as 020 or 16. | --fill=sequence |
| Memory Address Range | When Provide Range to fill is selected, enter the range here. Specify range as Start:End where Start and End use C syntax. Example 0x100:0x1FF is the same as 256:511. | --fill=sequence |
| ||