1.5.3.4.7 SRV_USER_PIB_SetRequest Function
C
void SRV_USER_PIB_SetRequest(uint16_t pibAttrib, void *pibValue, uint8_t pibSize);
Summary
Set a user PIB.
Description
This routine is used to set a user PIB.
Precondition
The SRV_USER_PIB_Initialize Function and SRV_USER_PIB_SetRequestCbRegister Function must have been called before.
Parameters
| Param | Description |
|---|---|
| pibAttrib | PIB attribute identifier |
| pibValue | PIB attribute value |
| pibSize | PIB attribute value size |
Returns
None.
Example
static void APP_SetRequestHandler(uint8_t setResult)
{
if (getResult == true)
{
...
}
}
int main(void)
{
int32_t resetValue = 0;
SRV_USER_PIB_Initialize();
SRV_USER_PIB_SetRequestCbRegister(APP_SetRequestHandler);
SRV_USER_PIB_SetRequest(PIB_USER_RESET_INFO, &resetValue, sizeof(resetValue));
}
Remarks
The result of setting the user PIB is returned in a callback function.