1.5.3.4.4 SRV_USER_PIB_GetRequestCbRegister Function
C
void SRV_USER_PIB_GetRequestCbRegister(SRV_USER_PIB_GET_REQUEST_CALLBACK callback);
Summary
Register a function to be called to get the requested user PIB.
Description
This routine allows a client to register an event handling function to be called when a requested user PIB is returned.
Precondition
The SRV_USER_PIB_Initialize Function must have been called before.
Parameters
| Param | Description |
|---|---|
| callback | Pointer to the callback function |
Returns
None.
Example
static void APP_GetRequestHandler(uint8_t getResult, uint16_t pibAttrib,
void *pibValue, uint8_t pibSize)
{
if (getResult == true)
{
...
}
}
int main(void)
{
SRV_USER_PIB_Initialize();
SRV_USER_PIB_GetRequestCbRegister(APP_GetRequestHandler);
}
Remarks
None.