5.3 Hold Function
The Suspend Serial Input (HOLD) pin is used to pause the serial communication with the device without having to stop or reset the clock sequence. The Hold mode, however, does not have an effect on the internal write cycle. Therefore, if a write cycle is in progress, asserting the HOLD pin will not pause the operation and the write cycle will continue to completion.
The Hold mode can only be entered while the CS pin is asserted. The Hold mode is activated by asserting the HOLD pin during the SCK low pulse. If the HOLD pin is asserted during the SCK high pulse, then the Hold mode will not be started until the beginning of the next SCK low pulse. The device will remain in the Hold mode as long as the HOLD pin and CS pin are asserted.
While in Hold mode, the SO pin will be in a high-impedance state. In addition, both the SI pin and the SCK pin will be ignored. The Write-Protect (WP) pin, however, can still be asserted or deasserted while in the Hold mode.
To end the Hold mode and resume serial communication, the HOLD pin must be deasserted during the SCK low pulse. If the HOLD pin is deasserted during the SCK high pulse, then the Hold mode will not end until the beginning of the next SCK low pulse.
0
’ state.