4.2 Generating the Filter Coefficients and Input Signal
(Ask a Question)Follow these steps:
- Launch the GUI and go to Filter Settings to generate the filter coefficients.
- Retain the default Filter
Generation parameters and select Generate Filter as
shown in the following figure.
Figure 4-1. Filter Generation Parameters - After generating the filter coefficients,
the Filter Response and the Filter Coefficient
plots are displayed as shown in the following figure.
Figure 4-2. Filter Response and Filter Coefficient - To generate the input signals, retain the
default parameters in the GUI and click Generate Signal as shown in
the following figure.
Figure 4-3. Generate Signal - The input signals and the frequency
spectrum of the specified signals are displayed in the Filter Input
tab, as shown in the following figure.
Figure 4-4. Filter Input Tab