4.1.1.1 BDB Commissioning APIs
BDB APIs related to commissioning is listed here
| Functions | |
| void | BDB_ConfigureInstallCode(ExtAddr_t deviceAddress, uint8_t
*installCode, IcStatusCallback_t pfCallback) This API calculates the CRC for the install code and compare with the given CRC. Derives the link key using SSP AES and sets the key in APS Key Pair Set |
| bool | BDB_InvokeCommissioning(BDB_InvokeCommissioningReq_t *req) The commissioning API invokes the commissioning based on the given information in the request structure |
| void | void BDB_ResetVia_TouchlinkCluster(ResetTargetCallback_t
pfcallback) Resets the target device to factory defaults using touchlink commissioning cluster. TBD-Whether such API is needed or not based on application defintion |
| void | BDB_SetInstallCodeUsage(bool useInstallCode) Sets the install code usage at the trust center |
| void | BDB_SetNodeJoinTimeout(uint8_t timeOutInSec) Sets the Node Join TimeOut |
| void | BDB_SetTCLKExchangeMethod(uint8_t exchangeMethod) Sets the TCLK Exchange Method BDB attribute |
| void | BDB_SetTCLKRetryMaxAttempts(uint8_t attempts) Sets the TCLK Retry Max Attempts BDB attribute |
| void | BDB_SetTCRequireKeyExchange(bool requireKeyExchange) Sets the Trust center Require key change or not of the joining device |
| void | BDB_SetToulinkRole(bool initiator) Sets the Touchlink role |