5.1.4.2 CS_ReadParameter Function
Syntax
void CS_ReadParameter(CS_MemoryItemId_t parameterId, void *memoryPtr);Description
This function gets the value of the parameter specified by its ID and writes it to the provided address in the memory.
The function reads the value of a CS parameter specified by its ID. A parameter ID is a constant;
the user can obtain its name by adding _ID suffix to the name of the
parameter. For example, the identifier of the CS_NWK_PANID parameter is
CS_NWK_PANID_ID.
The function copies the value to the location in memory specified by the second argument. For example, reading the extended address of the device is performed the following way:
ExtAddr_t ownExtAddr; CS_ReadParameter(CS_UID_ID, &ownExtAddr);
Input Parameters
| Parameter Name | Description |
|---|---|
[in] parameterId | ID of the parameter to be read |
[in] parameterId | A pointer where the parameter’s value is written |
Return Type and Values
- None