5.1.7.2.4 ZCL_StartSecurityReq Function
Syntax
void ZCL_StartSecurityReq(ZCL_StartSecurityReq_t *req);
Description
This function initializes the key establishment cluster, discovers the key establishment devices and performs the key establishment.
The applications supporting the key establishment cluster must call the function to perform key establishment procedures. The behavior differs between the trust center and common devices.
- On the trust center:
- If the user sets the
remoteAddressfield to ‘0’, the application initializes the key establishment cluster without performing key establishment with any device. - If the
remoteAddressfield is set to the extended address of a remote device, the trust center starts key establishment with it.
- If the user sets the
- On a common device:
- If the user sets the
remoteAddressfield to ‘0’ or to the extended address of the trust center, the key establishment with the trust center is going to start. - Otherwise, the request eventually fails. If not using the Certicom Security, the application always reports success status.
- If the user sets the
The response statuses, accessed via the argument’s
ZCL_StartSecurityConf_t-status field of the ZCL_StartSecurityReq_t-ZCL_StartSecurityConf callbacks argument, are as follows:- All possible status codes are wrapped in the
ZCL_SecurityStatus_tenumeration.
Input Parameters
| Parameter Name | Description |
|---|---|
req | Request structure to pass attribute id |
Return Type and Values
- None