14.2.1 Configuration Settings

The following table lists the description of the configuration parameters used in the hardware implementation of Sinc3 Filter. These are generic parameters and are varied as per the requirement of the application.

Table 14-2. Configuration Parameters
Signal NameDescription
g_STD_IO_WIDTHWidth of the input and output signals
g_DECIMATION_FACTOR

Division factor used to generate the decimated clock from the system clock input

g_BIPOLAR

Select 0, if ADC is unipolar

Select 1, if ADC is bipolar

g_NEGATE_OUTPUT

Select 0 if the data at the data_o port must be negated

Select 1 if the data at the data_o port must be passed through