1.2.1 Configuration of GUI Parameters

The following table lists the description of the configuration parameters used in the hardware implementation of ADC scaling. These are generic parameters and can be varied as per the requirement of the application.

Table 1-2. Configuration Parameters
Signal NameDescription
g_DEBUGWhen 0, supports Synthesis

When 1, supports Simulation

g_SIGNEDWhen 0, supports signed inputs from the ADC interface block

When 1, supports unsigned inputs from the ADC interface block

g_ADC_RESULTS_WIDTHDefines the width of the inputs from ADC measurements block
g_NO_MCYCLE_PATHDefines the number of clock delays required before asserting the multiplier done signal