4.4.1 Simulation
(Ask a Question)The following steps describe how to simulate the core using the testbench:
- Open the Libero SoC application, click
Catalog tab, expand
Solutions-MotorControl, double-click FOC
Transforms, and then click OK. The documentation
associated with the IP are listed under Documentation. Important: If you do not see the Catalog tab, navigate to menu and click Catalog to make it visible.
Figure 4-5. FOC Transformations IP Core in Libero SoC Catalog
- On the Stimulus Hierarchy
tab, click the testbench (
foc_transforms_tb.v), right click and then click .Important: If you do not see the Stimulus Hierarchy tab, navigate to menu and click Stimulus Hierarchy to make it visible.Figure 4-6. Simulating Pre-Synthesis Design
ModelSim opens with the testbench file as shown in the following figure.
Figure 4-7. ModelSim Simulation Window
Important: If the simulation is interrupted due to the
runtime limit specified in the
.do file, use the run
-all command to complete the simulation.