7.4.1 Simulation
(Ask a Question)The following steps describe how to simulate the core using the testbench:
- Open the Libero SoC application, click Libero SoC Catalog tab, expand Solutions-MotorControl
- Double-click T-Format Interface, and then click OK.
The documentation associated with the IP are listed under
Documentation. Important: If you do not see the Catalog tab, navigate to menu and click Catalog to make it visible.
Figure 7-6. T-Format Interface IP Core in Libero SoC Catalog - On the Stimulus Hierarchy
tab, right-click testbench (
t_format_interface_tb.v), point to , and then click Open Interactively.Important: If you do not see the Stimulus Hierarchy tab, navigate to menu and click Stimulus Hierarchy to make it visible.Figure 7-7. Simulating Pre-Synthesis Design ModelSim opens with the testbench file as shown in the following figure.
Figure 7-8. ModelSim Simulation Window
Important: If the simulation is interrupted due to the runtime limit specified in the
.do file, use the run -all command to complete the simulation.