6.4.1 Simulation
(Ask a Question)The following steps describe how to simulate the core using the testbench:
- Open the Libero SoC application, click Libero SoC Catalog tab, expand Solutions-MotorControl
- Double-click Median Filter, and then click OK. The documentation associated with the IP are listed under Documentation. Important: If you do not see the Catalog tab, navigate to menu and click Catalog to make it visible.
Figure 6-3. Median Filter IP Core in Libero SoC Catalog - On the Stimulus Hierarchy
tab, right-click testbench (
median_filter_tb.v), point to Simulate Pre-Synth Design , and then click Open Interactively.Important: If you do not see the Stimulus Hierarchy tab, navigate to menu and click Stimulus Hierarchy to make it visible.Figure 6-4. Simulating Pre-Synthesis Design ModelSim opens with the testbench file as shown in the following figure.
Figure 6-5. ModelSim Simulation Window
Important: If the simulation is interrupted due to the runtime limit specified in the
.do file, use the run -all command to complete the simulation.