3.4 Commonly Used Directives
There are several assembler directives that are typically used in each module. These have been used in the example code for this chapter and are discussed here.
Processor Directive
The PROCESSOR directive is not mandatory but should be used if the
assembler source in the module is only applicable to one device.
The
-mcpu option always specifies which device the code is being
built for. If the PROCESSOR directive has been used and there is a
mismatch between the device specified in that directive and in the option, an error
will be triggered. The line of code:PROCESSOR 18F47K42shows
the PIC18F47K42 device being specified. With this in place, the code cannot be built
for any other device.If your code can be built for multiple devices, the
PROCESSOR
directive should be omitted. You can instead make sections of your code specific to
the target device by using the preprocessor's conditional inclusion features and
preprocessor macros predefined by the PIC Assembler. For
example:#ifdef _18F47K40
movwf LATE
#endifwill assemble the
movwf instruction only for PIC18F47K40 devices. The
_18F47K40 preprocessor macro is one that is automatically
defined by the assembler, based on the device selected by the -mcpu
option. A full list of predefined macros is available in the MPLAB® XC8 PIC
Assembler User's Guide.End Directive
Use of the END directive is not mandatory, but
signifies an end to the source code in that module. There can be no further lines of
source present after an END directive, even blank ones.
If you use one or more
END directives in your program,
one (and only one) of those directives should specify the program's entry point
label to prevent an assembler warning being generated. This has been done in the
last line of the example
program:END resetVec