29.9.2 TUxyCON1
Note:
- Clock synchronization delays apply.
- This bit is held at zero if a
Start has occurred (the counter is “running”), but ERS is holding the counter at
the value zero when RESET =
‘b01(level-triggered). - The clearing of the ON bit in One Shot mode is subject to clock synchronization delays. Refer to the Synchronous vs. Asynchronous Operation and One Shot Mode sections for details.
- This bit is not clock synchronized
and only needs to be changed while ON =
0. - This bit is subject to clock synchronization delays. See Timer Counter and Capture Registers for details.
- If the counter is disabled (ON =
0) or if the module is frozen during debugging, then the timer clock has been disabled; the effect of setting CLR or CAPT command bits depends on the clock synchronization setting. If CSYNC =0, the corresponding action is performed immediately. If CSYNC =1, the corresponding action is delayed until the clock resumes (even in Frozen state while debugging). See also Timer Counter and Capture Registers. - A capture event can also be triggered by other means. See Timer Counter and Capture Registers for details.
- If the CAPT command is near-coincident with a Stop event, the captured value may represent the first event that occurs.
- The captured value is read by
setting RDSEL =
0and reading TUxyCR. - This bit may be set by software to invoke an interrupt or DMA operation.
- The interrupt flags will be set even if the corresponding interrupt is disabled.
- The PRIF interrupt will not occur if the user writes the PR value to the TUxyTMR counter register directly.
- The CIF interrupt trigger requires a running timer.
- This register is not available when the module is chained and operated as a Secondary module.
| Name: | TUxyCON1 |
| Bit | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 | |
| RUN | OSEN | CLR | LIMIT | CAPT | PRIF | ZIF | CIF | ||
| Access | R | R/W | R/S/HC | R/W | R/S/HC | R/W/HS | R/W/HS | R/W/HS | |
| Reset | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
Bit 7 – RUN Timer Run/Stop Status (Read-Only)(1,2)
| Reset States: |
|
| Value | Description |
|---|---|
| 1 | Timer is running (counting) and not being held in Reset by ERS (per EPOL bit selection) |
| 0 | Timer is not counting or is held in Reset by ERS |
Bit 6 – OSEN One Shot Mode Enable(3,4)
| Reset States: |
|
| Value | Description |
|---|---|
| 1 | The counter operates in One Shot mode; ON will be cleared by a Stop condition |
| 0 | The counter can be repeatedly started by the ERS signal |
Bit 5 – CLR Timer Counter “Clear” Command(5,6)
0’ has no effect.| Reset States: |
|
| Value | Description |
|---|---|
| 1 | Once set, the timer counter and the internal prescaler counter are cleared, then this bit is cleared (the captured value of TUxyCR is unchanged) |
| 0 | Clearing action is complete (or not started) |
Bit 4 – LIMIT Limit Mode Enable(4)
‘b00 (Continuous mode) and counter equals PR.| Reset States: |
|
| Value | Description |
|---|---|
| 1 | Counter value remains equal to PR (unchanged); no additional interrupts occur |
| 0 | Counter value goes tor PR+1 when clocked |
Bit 3 – CAPT Timer “Capture” Command(5,6,7,8,9)
0’ has no effect.| Reset States: |
|
| Value | Description |
|---|---|
| 1 | Once set, the counter value is captured in TUxyCR and this bit is cleared |
| 0 | TUxyCR update is complete (or not started) |
Bit 2 – PRIF Period Match Interrupt Flag(10,11,12)
| Reset States: |
|
| Value | Description |
|---|---|
| 1 | The counter has incremented from PR-1 to PR |
| 0 | The counter has not incremented from PR-1 to PR since this bit was last cleared |
Bit 1 – ZIF Zero Interrupt Flag(10,11)
| Reset States: |
|
| Value | Description |
|---|---|
| 1 | The counter has reset or rolled over to zero |
| 0 | The counter has not reset or rolled over since this bit was last cleared |
Bit 0 – CIF Capture Interrupt Flag(10,11,13)
| Reset States: |
|
| Value | Description |
|---|---|
| 1 | A capture event has occurred |
| 0 | A capture event has not occurred since this bit was last cleared |