44.7.5 ADC Module Core Control Registers
| Symbol | Description | Symbol | Description | Symbol | Description |
|---|---|---|---|---|---|
| R | Readable bit | HC | Cleared by Hardware | (Grey cell) | Unimplemented |
| W | Writable bit | HS | Set by Hardware | X | Bit is unknown at Reset |
| K | Write to clear | S | Software settable bit | — | — |
| Name: | CONFIG[0].CORCTRL |
| Offset: | 0x20 |
| Reset: | 0x00000C00 |
| Property: | Write-Protected, Enable-Protected |
| Bit | 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | |
| ADCDIV[6:0] | |||||||||
| Access | R/W | R/W | R/W | R/W | R/W | R/W | R/W | ||
| Reset | 0 | 0 | 0 | 0 | 0 | 0 | 0 | ||
| Bit | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | |
| SCNRTDS | STRGLVL | STRGSRC[3:0] | |||||||
| Access | R/W | R/W | R/W | R/W | R/W | R/W | |||
| Reset | 0 | 0 | 0 | 0 | 0 | 0 | |||
| Bit | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | |
| EIRQOVR | EIS[2:0] | SELRES[1:0] | SAMC[9:8] | ||||||
| Access | R/W | R/W | R/W | R/W | R/W | R/W | R/W | R/W | |
| Reset | 0 | 0 | 0 | 0 | 1 | 1 | 0 | 0 | |
| Bit | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 | |
| SAMC[7:0] | |||||||||
| Access | R/W | R/W | R/W | R/W | R/W | R/W | R/W | R/W | |
| Reset | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | |
Bits 30:24 – ADCDIV[6:0] Division Ratio for ADC Clock
ADCDIV provides the ADC analog functional clock referred to as the ADC clock or TAD, (i.e., the period of the ADC clock). It divides CTL_CLK output clock from (GCLK_ADC Period * (CTRLD.CTLCKDIV+1)) with period = TQ to produce the resulting ADC_CLK for ADC sampling and converting. It will have the period TAD given by the formula:
TAD = (GCLK_ADCx Period * (CTRLD.CTLCKDIV+1)) * (2 * ADCDIV)
Example 1:
TAD = 1/ADC_CLK = 1/(GCLK_ADCx Period * (CTRLD.CTLCKDIV+1)) * (2 * ADCDIV)
TAD = 1/ADC_CLK = 1/60 MHz = 16.6667 ns, SAMC = 0x4, SELRES = 0x3 = 12 bits, AIN0 active only.
ADC throughput rate:
FTPR = [1 / (6TAD + 13TAD)] / 1
= 1 / 19TAD
= 1 / (19 * 16.6667e-9)
= 3.157894 msps
Example 2: (Non Interleaved Mode)
TAD = 1/ADC_CLK = 1/(GCLK_ADCx Period * (CTRLD.CTLCKDIV+1)) * (2 * ADCDIV)
TAD = 1/ADC_CLK = 1/60 MHz = 16.6667 ns, SAMC = 0x4, SELRES = 0x3 = 12 bits, AIN0 and AIN3 in single ended mode active.
ADC throughput rate:
FTPR = [1 / (6TAD + 13TAD)] / 2
= (1 / 19TAD) / 2
= (1 / (16 * 16.6667e-9)) / 2
= 1.578947 msps
- This bit is Enabled Protected : (Writes are ignored when CTRLA.ENABLE = 1) . Returns a bus error.
- The minimum sample rate for ADC is Ftpr >= 100 ksps.
| Value | Description |
|---|---|
| 1111111 | 254·TQ = TAD |
| ... | ... |
| 0000011 | 6·TQ = TAD |
| 0000010 | 4·TQ = TAD |
| 0000001 | 2·TQ = TAD |
| 0000000 | Reserved |
Bit 22 – SCNRTDS SCAN Retrigger Disable for ADC
- This bit is Enabled Protected: (Writes are ignored when CTRLA.ENABLE = 1). Returns a bus error.
| Value | Description |
|---|---|
| 0 | Allows the scan cycle to restart from the beginning, lowest CSSn channel even before all of the scan channels have been measured if a new scan trigger arrives before then. If this happens then the INTENCLRn.EOSRDY flag will be set when the current scan is interrupted, and the new scan starts from the beginning of the lowest CSSn channel selected. |
| 1 | Prevents an early scan trigger (arriving before of the end of the current scan) from starting a new scan cycle. The scan will includes all channels associated with ADCn which have their CHNCFG4n.TRGSRCk set to point to the Scan Trigger, i.e., CHNCFG4n.TRGSRCy[3:0] = 4’b0011, and have their associated CHNCFG2n.CSSk bit set. |
Bit 21 – STRGLVL Scan Trigger High Level Sensitivity for the ScanTrigger of the ADCn (STRIGn)
- This bit is Enabled Protected (Writes are ignored when CTRLA.ENABLE = 1). Returns a bus error.
STRGLVL functions as follows:
| Value | Description |
|---|---|
| 0 | SCANTRG is Positive Edge Active(the power-up value for
backwards compatibility). A positive edge on the SCANTRG will initiate a single but complete scan of all included channels. |
| 1 | SCANTRG is High Level Active. So long as SCANTRG stays high, the entire scan will re-trigger. |
Bits 19:16 – STRGSRC[3:0] SCAN Trigger Source Select for the SCANTRG
These bits select the trigger source for the scan trigger SCANTRG serving ADCn. The trigger STRIGn serves all the channels k which are associated to ADCn, have their CHNCFG{4|5}n.TRGSRCk = 4’h0011, and have their Channel Scan Select bit set (CHNCFG2n.CSSk = 1’b1).
- This bit is Enabled Protected: (Writes are ignored when CTRLA.ENABLE = 1). Returns a bus error.
| Value | Description |
|---|---|
| 0000 | No trigger (NOP) |
| 0001 | Global Software Trigger (CTRLB.GSWTRG) - self-cleared on the next APB clock cycle. |
| 0010 | Level Software Trigger (CTRLB.LSWTRG) - NOT self-cleared. |
| 0011 | Reserved |
| 0100 | Synchronous Trigger (CTRLC.CNT) Note: In order to utilize
CORCTRL.STRGSRC = 0x4, the user must configure the following
registers:
|
| 0101 - 1111 | ADC Trigger Event User 0 – 10 |
Bit 15 – EIRQOVR Interrupt Type Selection
- This bit is Enabled Protected: (Writes are ignored when CTRLA.ENABLE = 1). Returns a bus error.
| Value | Description |
|---|---|
| 0 | Use normal ADC interrupts |
| 1 | Use early ADC interrupts as defined by CORCTRLn.EIS bits |
Bits 14:12 – EIS[2:0] Early Interrupt Select Bits for ADCn
These bits select the number of core clocks and TAD clocks prior to the end of conversion at which the early interrupt is generated. All channels serviced by ADCn share the same EIS setting.
The interrupt is generated ((EIS +1) x TAD) ADC Module clocks prior to end of conversion.
- This bit is Enabled Protected: (Writes are ignored when CTRLA.ENABLE = 1). Returns a bus error.
- Early interrupt is a
feature that can be useful in ADC very high speed data acquisitions to
mask the MCU interrupt latency delay.
Example: CPU MCLK =200 MHz, ADC CTL_CLK = 60 MHz and ADC TAD Clk = 30 MHz.
Hypothetically, if it took the CPU 20 MCLK cycles to service an interrupt, then theoretically the ADC early interrupt EIS could be set to 4, so that the ISR latency was masked. The CPU could then read the ADC result almost immediately from within the Interrupt Service Routine (ISR), when the result was ready, without any concern for overwriting the current result or FIFO with the next ADC conversion result.
- 12-bit Resolution, all 8 possible settings are allowed, 0 - 7
- 10-bit Resolution, all 8 possible settings are allowed, 0 - 7
- 8-bit Resolution, only the 6 lowest settings are allowed, 0 - 5
- 6-bit Resolution, only the 4 lowest settings are allowed, 0 - 3
The hardware will utilize the maximum allowed EIS setting if the user sets the EIS value that is too big.
| Value | Description |
|---|---|
| 0x0 | Generate interrupt 1 TAD clock before end of ADC conversion |
| 0x1 | Generate interrupt 2 TAD clocks before end of ADC conversion |
| 0x2 | Generate interrupt 3 TAD clocks before end of ADC conversion |
| 0x3 | Generate interrupt 4 TAD clocks before end of ADC conversion |
| 0x4 | Generate interrupt 5 TAD clocks before end of ADC conversion |
| 0x5 | Generate interrupt 6 TAD clocks before end of ADC conversion |
| 0x6 | Generate interrupt 7 TAD clocks before end of ADC conversion |
| 0x7 | Generate interrupt 8 TAD clocks before end of ADC conversion |
Bits 11:10 – SELRES[1:0] ADC Resolution for the ADCn
- This bit is Enabled Protected: (Writes are ignored when CTRLA.ENABLE = 1). Returns a bus error.
| Value | Description |
|---|---|
| 00 | 6 bits |
| 01 | 8 bits |
| 10 | 10 bits |
| 11 | 12 bits (power-on default) |
Bits 9:0 – SAMC[9:0] Sample Count
The sample time required depends on the external analog signal source impedance. Refer to the ADC electrical characteristics of SAMC values required based on external source impedance. If the external analog source impedance is unknown or if your getting inconsistent ADC results consider increasing the SAMC sample time at the cost of a lower ADC throughput rate of course.
ADCn Throughput Rate:
FTPR = [1 / ((SAMC value +2) * TAD) + ((#bits of resolution selected+1)*TAD)] / # of active AINx inputs on ADCn
- All channels serviced by ADCn share the same SAMC setting.
- The sampling sequence starts with a trigger event.
- The internal sampling cap is not discharged between samples. These bits are Enabled Protected: Writes are ignored when CTRLA.ENABLE = 1 returns a bus error.
- When IVREF is to be sampled ( Internal - ADC3 Module - Channel 6), (SAMC value + 2) * TAD must be ≧ 30 us.
| Value | Description |
|---|---|
| 1111111111 | 1025 TADn |
| ... | ... |
| 0000000001 | 3 TADn |
| 0000000000 | Reserved |