32.8.5 Network Control Register

Table 32-20. Register Bit Attribute Legend
SymbolDescriptionSymbolDescriptionSymbolDescription
RReadable bitHCCleared by Hardware(Grey cell)Unimplemented
WWritable bitHSSet by HardwareXBit is unknown at Reset
KWrite to clearSSoftware settable bit
Name: NCR
Offset: 0x1000
Reset: 0x00000000
Property: Read/Write

Bit 3130292827262524 
          
Access  
Reset  
Bit 2322212019181716 
     LPIFNPTXPBPFENPBPR 
Access R/WR/WR/WR/W 
Reset 0000 
Bit 15141312111098 
 SRTSM  TXZQPFTXPFTHALTTSTARTBP 
Access R/WR/WR/WR/WR/WR/W 
Reset 000000 
Bit 76543210 
 WESTATINCSTATCLRSTATMPETXENRXENLBL  
Access R/WR/WR/WR/WR/WR/WR/W 
Reset 0000000 

Bit 19 – LPI Low Power Idle Transmission Enable

When this bit is set, LPI (low power idle) is immediately transmitted. LPI is transmitted even if transmit enable bit NCR.TXEN is disabled.

Setting this bit also sends a pause signal to the transmit datapath.

Bit 18 – FNP Flush Next Packet

Writing a '1' to this bit will flush the next packet from the System RAM. Flushing the next packet will only take effect if the DMA is not currently writing a packet already stored in the DPRAM to memory.

Bit 17 – TXPBPF Transmit PFC Priority-based Pause Frame

Takes the values stored in the Transmit PFC Pause Register.

Bit 16 – ENPBPR Enable PFC Priority-based Pause Reception

Writing a '1' to this bit enables PFC Priority Based Pause Reception capabilities, enabling PFC negotiation and recognition of priority-based pause frames.

ValueDescription
0Normal operation
1PFC Priority-based Pause frames are recognized.

Bit 15 – SRTSM Store Receive Time Stamp to Memory

Writing a '1' to this bit causes the CRC of every received frame to be replaced with the value of the nanoseconds field of the 1588 timer that was captured as the receive frame passed the message time stamp point.

Note that bit RFCS in register NCFGR may not be set to 1 when the timer should be captured.

ValueDescription
0Normal operation
1All received frames' CRC is replaced with a time stamp.

Bit 12 – TXZQPF Transmit Zero Quantum Pause Frame

Writing a '1' to this bit causes a pause frame with zero quantum to be transmitted.

Writing a '0' to this bit has no effect.

Bit 11 – TXPF Transmit Pause Frame

Writing one to this bit causes a pause frame to be transmitted.

Writing a '0' to this bit has no effect.

Bit 10 – THALT Transmit Halt

Writing a '1' to this bit halts transmission as soon as any ongoing frame transmission ends.

Writing a '0' to this bit has no effect.

Bit 9 – TSTART Start Transmission

Writing a '1' to this bit starts transmission.

Writing a '0' to this bit has no effect.

Bit 8 – BP Back Pressure

In 10M or 100M half duplex mode, writing a '1' to this bit forces collisions on all received frames.

ValueDescription
0Frame collisions are not forced.
1Frame collisions are forced in 10M and 100M half duplex mode.

Bit 7 – WESTAT Write Enable for Statistics Registers

Writing a '1' to this bit makes the statistics registers writable for functional test purposes.

ValueDescription
0Statistics Registers are write-protected.
1Statistics Registers are write-enabled.

Bit 6 – INCSTAT Increment Statistics Registers

Writing a '1' to this bit increments all Statistics Registers by one for test purposes.

Writing a '0' to this bit has no effect.

This bit will always read '0'.

Bit 5 – CLRSTAT Clear Statistics Registers

Writing a '1' to this bit clears the Statistics Registers.

Writing a '0' to this bit has no effect.

This bit will always read '0'.

Bit 4 – MPE Management Port Enable

Writing a '1' to this bit enables the Management Port.

Writing a '0' to this bit disables the Management Port, and forces MDIO to high impedance state and MDC to low impedance.

ValueDescription
0Management Port is disabled.
1Management Port is enabled.

Bit 3 – TXEN Transmit Enable

Writing a '1' to this bit enables the ETH transmitter to send data.

Writing a '0' to this bit stops transmission immediately, the transmit pipeline and control registers is cleared, and the Transmit Queue Pointer Register will be set to point to the start of the transmit descriptor list.
Note: The TXEN and RXEN bits should not be set (enabled) until all other NCR settings are completed.
ValueDescription
0Transmit is disabled.
1Transmit is enabled.

Bit 2 – RXEN Receive Enable

Writing a '1' to this bit enables the ETH to receive data.

Writing a '0' to this bit stops frame reception immediately, and the receive pipeline is cleared. The Receive Queue Pointer Register is not affected.
Note: The TXEN and RXEN bits should not be set (enabled) until all other NCR settings are completed.
ValueDescription
0Receive is disabled.
1Receive is enabled.

Bit 1 – LBL Loop Back Local

Writing '1' to this bit connects ETH_TX to ETH_RX, ETH_TXEN to ETH_RXDV, and forces full duplex mode.

ETH_RXCK and ETH_TXCK may malfunction as the ETH is switched into and out of internal loop back. It is important that receive and transmit circuits have already been disabled when making the switch into and out of internal loop back.

ValueDescription
0Loop back local is disabled.
1Loop back local is enabled.