26.7.4.3 Linked List Step Tracing
The channel will set the SD, CC, BH, BC interrupt flags as described in Block Transfer. The user can track progress through a linked-list by monitoring interrupts based on one of these interrupt flags such as the BC. This is useful if the software needs to be kept up-to-date with the progress of the linked-list execution.