These bits are cleared when the corresponding backup I/O pin detects a logical low level on the input pin or when the backup I/O is not enabled.
These bits are set when the corresponding backup
I/O pin detects a logical high level on the input pin when the backup I/O is
enabled.
| BKIN[2:0] | PAD | Description |
|---|
| BKIN[0] | PSOK | If
BBPS.PSOKEN=1, BKIN[0] will give the input value of the PSOK pin |
| BKIN[1] | OUT[0] | If
BKOUT.EN[0]=1, BKIN[1] will give the input value of the OUT[0]
pin |
| BKIN[2] | OUT[1] | If
BKOUT.EN[1]=1, BKIN[2] will give the input value of the OUT[1]
pin |