The ERPS instances are configured on the ERPS Configuration page. To
configure ERPS, go to Configuration > ERPS . The ERPS
configuration page is displayed. Figure 4-25. ERPS Configuration
To configure EPRS, click the + icon at the bottom right
corner. The ERPS Configuration options are displayed.
Figure 4-26. ERPS Configuration Table
The list of configuration parameters are as follows:
Configuration:
ERPS #: The ID of ERPS. The allowed value is from 1:64.
Version: ERPS protocol version. v1 and v2 are supported.
Type: Type of ring. The following are the possible values:
Major: ERPS major ring (G.8001-2016, clause 3.2.39)
Sub: ERPS sub-ring (G.8001-2016, clause 3.2.66)
InterSub: ERPS sub-ring on an interconnection node (G.8001-2016, clause 3.2.66)
VC: Controls whether to use a Virtual Channel with a sub-ring
Interconnect Instance: For a sub-ring on an interconnection node, this must refer the instance ID of the ring to which this sub-ring is connected.
Interconnect Prop: Controls whether the ring referenced by Interconnect Instance shall propagate R-APS flush PDUs whenever this sub-ring's topology changes.
Ring ID: The Ring ID is used. Along with the control VLAN, this is used to identify R-APS PDUs as belonging to a particular ring.
Node ID: The Node ID is used inside the R-APS specific PDU to uniquely identify this node (switch) on the ring
Level: MD/MEG Level of R-APS PDUs that are transmitted
Control VLAN: The VLAN on which R-APS PDUs are transmitted and received on the ring ports
Control PCP: The PCP value used in the VLAN tag of the R-APS PDUs
Rev: Revertive (true) or Non-Revertive (false) mode
Guard: Guard time in ms. The valid range is 10 ms–2000 ms
WTR: Wait-to-Restore time in seconds. Valid range 1s–720s
Hold Off: Hold off time in ms. Value is rounded down to 100 ms precision. Valid range is 0 ms–10000 ms.
Enable: The administrative state of this ERPS. Check to make it function normally and uncheck to make it stop functioning.
Signal Fail Trigger:
Type: Selects whether
Signal Fail (SF) comes from the link state of a given interface or from a
Down-MEP.
Domain,
Service, MEPID: Identification of the MEP instance to provide
SF, if Type is MEP.
Protected VLANs: VLANs, which
are protected by this ring instance. At least one VLAN must be protected. Specify as
a comma-separated list of VLAN numbers or VLAN ranges. For example, 1, 4, 7,
30–70.
Ring Protection Link:
RPL Mode: The following Ring Protection Link modes are available:
None: This switch does not have the RPL port in the ring
Owner: This switch is RPL owner for the ring (G.8001-2016,
clause 3.2.61)
Neighbor: This switch is RPL neighbor for the ring
(G.8001-2016, clause 3.2.60)
RPL Port: Allows you to select the east (port 0) or west (port 1) as
the RPL block. This is not used if the RPL mode is None.