4.33 GVRP Configuration
The following sections describe the GVRP Configurations.
The GVRP Configuration page has the following parameters:
- Enable GVRP: To enable the GVRP feature globally, select this check box and click Save.
- GVRP protocol timers:
- Join-time is a value in the range of 1-20cs, that is in units of 1/100 of a second. The default value is 20cs.
- Leave-time is a value in the range of 60-300cs, the default is 60cs.
- Leave All-time is a value in the range of 1000-5000cs, the default is 1000cs.
- Max VLANs: When GVRP is enabled, a max number of VLANs supported by GVRP is specified. By default, this number is 20. This number can only be changed when GVRP is turned off.