Configure DHCPv6 (that is, DHCP over IPv6) Snooping and Relay on the Configuration > DHCPv6 > Snooping page.
DHCP Snooping Configuration:
The following figure shows a DHCPv6 Snooping configuration. Figure 4-30. DHCPv6 Snooping ConfigurationThe list of parameters is as follows:
Snooping Mode: Indicates the DHCPv6 snooping mode. The following are the possible modes:
Enabled: Enables DHCPv6 snooping mode operation. When DHCPv6 snooping mode operation is enabled, the DHCPv6 client request messages are forwarded to trusted ports and only allow reply packets from trusted ports.
Disabled: Disables DHCP snooping mode operation
Unknown IPv6 Next-Headers: Indicates how Unknown IPv6 Next-Header values must be treated. The switch must parse all IPv6 packets to a DHCPv6 client to determine if it is a DHCPv6 message. If an unknown IPv6 extension header is encountered, then the parsing cannot continue. See RFC 7610, section 5, item 3 for details. Following are the possible available options:
Drop: Drops packets with unknown IPv6 extension headers. This is the most secure option but may result in traffic disruptions.
Allow: Allows packets with unknown IPv6 extension headers. This is a less secure option but prevents traffic disruptions.
Port Mode Configuration: Indicates the DHCPv6 snooping port mode. Possible port modes are:
Trusted: Configures the port as trusted source of the DHCPv6 messages
Untrusted: Configures the port as untrusted source of the DHCPv6 messages
DHCP Relay Configuration
This is a table to configure DHCPv6_Relay for a specific VLAN
Figure 4-31. DHCPv6 Relay
Configuration
The list of parameters is as follows:
Interface:
Interface identification.
Relay
Interface: Interface identification. The id of the interface
used for relaying.
Relay
Destination: An Ipv6 address represented as human readable test
as specified in RFC5952. The IPv6 address of the DHCPv6 server that requests
shall be relayed to. The default value 'ff05::1:3’ means 'any DHCP server'.