6.2 ICICLE Kit
(Ask a Question)To start the OPC UA server on the ICICLE Kit, perform the following steps:
- Program the job file on the ICICLE Kit. For more information on installing the job file, see Programming the Device.
- Install the wic image on the ICICLE Kit. For more information on installing the wic image, see Flashing Linux .wic Image in eMMC Mode.
- Reboot and login as root.
- Check the IP address of the machine. Note and keep the IP address handy.
- Connect the Stepper Motor to the Stepper 7 Click Board.
- Connect the Stepper 7 Click Board to the Mikro Bus Connector.
- Navigate to the /opt/microchip/opcua/icicle-kit/ folder.
- Execute the
./icicle-motor-server.py &orpython3 icicle-motor-server.py &command. It displays the following message:Attempting to load the MCP23S08 SPI device MCP23S08 SPI device loaded successfullyWait for the terminal to display the following log:
Stepper Motor - OPC-UA Server StartedThe server starts and runs in the background at port
4840. - Connect to the OPC UA server using the UAExpert OPC UA client. For information on connecting to the server, see Establishing a Connection Between OPC UA and Client/Server.