1.21 SPI Blocking
This example application demonstrates how to use the SPI peripheral to transmit and receive a block of data in a blocking manner.
Description
This example demonstrates the transmit and receive operation over SPI interface in a blocking manner. The example application transmits known values from an array and verifies the data received through the loop back by comparing the transmitted data and the received data. The example application performs the loop back test only once after a power on reset. After the loop back is complete, the status of the loop back is indicated and the application remains idle. The loop back test requires the MOSI output pin to be connected to the MISO input pin so that anything transmitted will also be received.
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/spi/spi_self_loopback_blocking/firmware.
To build the application, refer to the following table and open the project using its IDE.
Project Name | Description |
---|---|
pic32mx470_curiosity.X | MPLABX project for Curiosity PIC32MX470 Development Board |
pic32mx_xlp_sk.X | MPLABX project for PIC32MX274 XLP Starter Kit |
Setting Up the Hardware
The following table shows the target hardware for the application projects.
Project Name | Description |
---|---|
pic32mx470_curiosity.X | Curiosity PIC32MX470 Development Board |
pic32mx_xlp_sk.X | PIC32MX274 XLP Starter Kit |
Setting Up Curiosity PIC32MX470 Development Board
- Use a jumper wire to short pin MOSI and pin MISO of the J10 connector
- Connect mini USB cable to the ‘Debug USB’ connector(J3) on the board to the
computerNote: Ensure that the series resistors on the mikroBUS headers are of value 0 Ohms.
Setting Up PIC32MX274 XLP Starter Kit
- Use a jumper wire to short pin MOSI and pin MISO of the J5 connector
- Connect micro USB cable to the ‘Debug USB’ connector(J9) on the board to the computer
Running the Application
- Build and program the application using its IDE
- LED indicates the success or failure:
- LED is turned ON when the when the value received matched with the transmitted value
- LED is turned OFF when the when the value received did not match with the transmitted value
Board | LED Name |
---|---|
Curiosity PIC32MX470 Development Board | LED1 |
PIC32MX274 XLP Starter Kit | LED1 (RED) |