1.19 RCON Reset Handler

This example shows how to use the RCON peripheral to indicate the cause of the device reset and clear the reset causes.

Description

The Reset module combines all Reset sources and controls the device Host Reset signal, SYSRST. The Reset module allows the reset source to be identified and it clears the reset cause through software. The following is a list of device Reset sources:

  • POR: Power-on Reset
  • MCLR: Host Clear Reset pin
  • SWR: Software Reset
  • WDTR: Watchdog Timer Reset
  • BOR: Brown-out Reset
  • CMR: Configuration Mismatch Reset
  • HVDR: High Voltage Detect Reset

This example application uses the RCON peripheral to indicate the MCLR and the Watchdog reset. The WDT reset is emulated by not feeding the watchdog on switch press.

Downloading and Building the Application

To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.

Path of the application within the repository is apps/rcon/reset_handler/firmware.

To build the application, refer to the following table and open the project using its IDE.

Project NameDescription
pic32mx470_curiosity.XMPLABX project for Curiosity PIC32MX470 Development Board

Setting Up the Hardware

The following table shows the target hardware for the application projects.

Project NameDescription
pic32mx470_curiosity.XCuriosity PIC32MX470 Development Board

Setting Up Curiosity PIC32MX470 Development Board

  • To run the demo, the following additional hardware are required:
  • Connect mini USB cable to the ‘Debug USB’ connector(J3) on the board to the computer
  • Install an USB UART click board on to the mikroBUS socket J5
  • Connect mini USB cable between PC and the USB UART click board
    Note: Ensure that the series resistors on the mikroBUS headers are of value 0 Ohms.

Running the Application

  1. Open the Terminal application (Ex.: Tera term) on the computer
  2. Connect to the “USB to UART” COM port and configure the serial settings as follows:
    • Baud : 115200
    • Data : 8 Bits
    • Parity : None
    • Stop : 1 Bit
    • Flow Control : None
  3. Build and Program the application project using its IDE
  4. Following message is output on console:
  5. Watch timer is fed periodically using Core Timer to prevent the WDT reset and the LED is toggled
  6. Press the switch to put the system in deadlock
  7. LED should stop blinking and the console should print the following message
  8. The WDT will reset the device in four seconds and the demonstration should restart