1.17 NVM Flash Read Write

This example application demonstrates how to use the NVM to erase and program the internal Flash memory.

Description

This example uses the NVM peripheral library to erase a page and write an array of values to the internal Flash memory. It verifies the value written by reading the values back and comparing it to the value written.

Downloading and Building the Application

To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.

Path of the application within the repository is apps/nvm/flash_read_write/firmware.

To build the application, refer to the following table and open the project using its IDE.

Project NameDescription
pic32mx470_curiosity.XMPLABX project for Curiosity PIC32MX470 Development Board
pic32mx_eth_sk2.XMPLABX project for PIC32 Ethernet Starter Kit
pic32mx_xlp_sk.XMPLABX project for PIC32MX274 XLP Starter Kit
pic32mx_sk.XMPLABX project for PIC32MX Starter Kit

Setting Up the Hardware

The following table shows the target hardware for the application projects.

Project NameDescription
pic32mx470_curiosity.XCuriosity PIC32MX470 Development Board
pic32mx_eth_sk2.XPIC32 Ethernet Starter Kit
pic32mx_xlp_sk.XPIC32MX274 XLP Starter Kit
pic32mx_sk.XPIC32MX Starter Kit

Setting Up Curiosity PIC32MX470 Development Board

  • Connect mini USB cable to the ‘Debug USB’ connector(J3) on the board to the computer

Setting Up PIC32 Ethernet Starter Kit

  • Connect mini USB cable to the ‘Debug USB’ connector(J7) on the board to the computer

Setting Up PIC32MX274 XLP Starter Kit

  • Connect micro USB cable to the ‘Debug USB’ connector(J9) on the board to the computer

Setting Up PIC32MX Starter Kit

  • Connect mini USB cable to the ‘Debug USB’ connector(J1) on the board to the computer