2.2.5 MCC Configuration
The following figure provides an overview of the MCC Project Graph:
- The EIC peripheral is used for the
two user switches (EIC 0 and EIC 1) and for the DALI stack (EIC 15):
Figure 2-5. EIC Module SW1 is routed to the PD00 pin, and SW2 is routed to the PD01 pin:
Figure 2-6. EIC Pins 0 and 1 Configuration DALI RX interrupt is routed to the PC31 pin:
Figure 2-7. EIC Pin 15 Configuration - The SERCOM4 peripheral is used for
console communication through a USB cable:
Figure 2-8. SERCOM4 Module The following pins are used for serial communication:
Figure 2-9. SERCOM4 Pins Configuration - SERCOM7 is used for communication
with the LTE IoT module:
Figure 2-10. SERCOM7 Module The pins used are:
Figure 2-11. SERCOM7 Pins Configuration - The TC0 peripheral is used for the
LTEIoT task:
Figure 2-12. TC0 Module - The TC4 peripheral is used by the
DALI stack:
Figure 2-13. TC4 Module - The ADC0 peripheral is used for the
motion sensor:
Figure 2-14. ADC0 Module Pin configuration:
Figure 2-15. ADC0 Pins Configuration - The ADC1 peripheral is used for the
ambient light sensor:
Figure 2-16. ADC1 Module Pin configuration:
Figure 2-17. ADC1 Pins Configuration - The SysTick is used to execute
various operations at a specific interval:
Figure 2-18. SysTick Module