3.13 Input Capture Driver
Overview
Input Capture is used to capture a timer value from an independent timer base on the occurrence of an event on an input pin. This is useful in applications requiring frequency (time period) and pulse measurement.
Features
- User configurable capture mode like any Edge Detect or Every Raising Edge or Every Falling Edge.
- Independent timer period depends on the clock source selected from the PLIB.
- In sync operation, the timer Reset or clear occurs when the input selected by SYNC is asserted,in trigger operation, the timer is held in Reset until the input selected by trigger is asserted.
3.13.1 Module Documentation
3.13.1.1 Input Capture Driver
Input Capture Driver is a 16-bit timer or 32-bit timer that is useful in applications requiring frequency (time period) and pulse measurement using dsPIC MCUs.
3.13.1.1.1 Module description
Input Capture Driver is a 16-bit timer or 32-bit timer that is useful in applications requiring frequency (time period) and pulse measurement using dsPIC MCUs.
Data structures
struct INPUT_CAPTURE_INTERFACE
Structure containing the function pointers of MCCP-InputCapture driver.
Definitions
#define Input_Capture2_Initialize SCCP2_InputCapture_Initialize
This macro defines the Custom Name for SCCP2_InputCapture_Initialize API.
#define Input_Capture2_Deinitialize SCCP2_InputCapture_Deinitialize
This macro defines the Custom Name for SCCP2_InputCapture_Deinitialize API.
#define Input_Capture2_Start SCCP2_InputCapture_Start
This macro defines the Custom Name for SCCP2_InputCapture_Start API.
#define Input_Capture2_Stop SCCP2_InputCapture_Stop
This macro defines the Custom Name for SCCP2_InputCapture_Stop API.
#define Input_Capture2_Tasks SCCP2_InputCapture_Tasks
This macro defines the Custom Name for SCCP2_InputCapture_Tasks API.
#define Input_Capture2_DataRead SCCP2_InputCapture_DataRead
This macro defines the Custom Name for SCCP2_InputCapture_DataRead API.
#define Input_Capture2_HasBufferOverflowed SCCP2_InputCapture_HasBufferOverflowed
This macro defines the Custom Name for SCCP2_InputCapture_HasBufferOverflowed API.
#define Input_Capture2_IsBufferEmpty SCCP2_InputCapture_IsBufferEmpty
This macro defines the Custom Name for SCCP2_InputCapture_IsBufferEmpty API.
#define Input_Capture2_OverflowFlagClear SCCP2_InputCapture_OverflowFlagClear
This macro defines the Custom Name for SCCP2_InputCapture_OverflowFlagClear API.
#define Input_Capture2_InputCapture_CallbackRegister SCCP2_InputCapture_CallbackRegister
This macro defines the Custom Name for SCCP2_InputCapture_CallbackRegister API.
Functions
void SCCP2_InputCapture_Initialize (void)
Initializes the SCCP2-InputCapture module.
void SCCP2_InputCapture_Deinitialize (void)
Deinitializes the SCCP2-InputCapture to POR values.
void SCCP2_InputCapture_Start (void)
Starts the InputCapture operation.
void SCCP2_InputCapture_Stop (void)
Stops the InputCapture operation.
void SCCP2_InputCapture_CallbackRegister (void(*handler)(void))
This function can be used to override default callback and to define custom callback for SCCP2 InputCapture event.
void SCCP2_InputCapture_Callback (void)
This is the default callback with weak attribute. The user can override and implement the default callback without weak attribute or can register a custom callback function using SCCP2_InputCaptureCallbackRegister.
uint32_t SCCP2_InputCapture_DataRead (void)
Reads the captured value.
bool SCCP2_InputCapture_HasBufferOverflowed (void)
Returns the buffer overflow status.
bool SCCP2_InputCapture_IsBufferEmpty (void)
Returns the buffer empty status.
void SCCP2_InputCapture_OverflowFlagClear (void)
Clears the buffer overflow status flag.
Variables
const struct INPUT_CAPTURE_INTERFACE Input_Capture2
Structure object of type INPUT_CAPTURE_INTERFACE with the custom name given by the user in the Melody Driver User interface. The default name e.g. Input_Capture1 can be changed by the user in the INPUT_CAPTURE user interface. This allows defining a structure with application specific name using the 'Custom Name' field. Application specific name allows the API Portability.
3.13.1.1.2 Definition Documentation
Input_Capture2_DataRead
#define Input_Capture2_DataRead SCCP2_InputCapture_DataRead
This macro defines the Custom Name for SCCP2_InputCapture_DataRead API.
Input_Capture2_Deinitialize
#define Input_Capture2_Deinitialize SCCP2_InputCapture_Deinitialize
This macro defines the Custom Name for SCCP2_InputCapture_Deinitialize API.
Input_Capture2_HasBufferOverflowed
#define Input_Capture2_HasBufferOverflowed SCCP2_InputCapture_HasBufferOverflowed
This macro defines the Custom Name for SCCP2_InputCapture_HasBufferOverflowed API.
Input_Capture2_Initialize
#define Input_Capture2_Initialize SCCP2_InputCapture_Initialize
This macro defines the Custom Name for SCCP2_InputCapture_Initialize API.
Input_Capture2_InputCapture_CallbackRegister
#define Input_Capture2_InputCapture_CallbackRegister SCCP2_InputCapture_CallbackRegister
This macro defines the Custom Name for SCCP2_InputCapture_CallbackRegister API.
Input_Capture2_IsBufferEmpty
#define Input_Capture2_IsBufferEmpty SCCP2_InputCapture_IsBufferEmpty
This macro defines the Custom Name for SCCP2_InputCapture_IsBufferEmpty API.
Input_Capture2_OverflowFlagClear
#define Input_Capture2_OverflowFlagClear SCCP2_InputCapture_OverflowFlagClear
This macro defines the Custom Name for SCCP2_InputCapture_OverflowFlagClear API.
Input_Capture2_Start
#define Input_Capture2_Start SCCP2_InputCapture_Start
This macro defines the Custom Name for SCCP2_InputCapture_Start API.
Input_Capture2_Stop
#define Input_Capture2_Stop SCCP2_InputCapture_Stop
This macro defines the Custom Name for SCCP2_InputCapture_Stop API.
Input_Capture2_Tasks
#define Input_Capture2_Tasks SCCP2_InputCapture_Tasks
This macro defines the Custom Name for SCCP2_InputCapture_Tasks API.
3.13.1.1.3 Function Documentation
SCCP2_InputCapture_Callback()
void SCCP2_InputCapture_Callback (void )
This is the default callback with weak attribute. The user can override and implement the default callback without weak attribute or can register a custom callback function using SCCP2_InputCaptureCallbackRegister.
| none |
none |
SCCP2_InputCapture_CallbackRegister()
void SCCP2_InputCapture_CallbackRegister (void(*)(void) handler)
This function can be used to override default callback and to define custom callback for SCCP2 InputCapture event.
| in | handler |
- Address of the callback function |
none |
SCCP2_InputCapture_DataRead()
uint32_t SCCP2_InputCapture_DataRead (void )
Reads the captured value.
SCCP2_InputCapture_Initialize must be called. |
| none |
Returns the captured value |
SCCP2_InputCapture_Deinitialize()
void SCCP2_InputCapture_Deinitialize (void )
Deinitializes the SCCP2-InputCapture to POR values.
| none |
none |
SCCP2_InputCapture_HasBufferOverflowed()
bool SCCP2_InputCapture_HasBufferOverflowed (void )
Returns the buffer overflow status.
SCCP2_InputCapture_Initialize must be called |
| none |
true - input capture buffer has overflowed false - input capture buffer has not overflowed |
SCCP2_InputCapture_Initialize()
void SCCP2_InputCapture_Initialize (void )
Initializes the SCCP2-InputCapture module.
| none |
none |
SCCP2_InputCapture_IsBufferEmpty()
bool SCCP2_InputCapture_IsBufferEmpty (void )
Returns the buffer empty status.
SCCP2_InputCapture_Initialize must be called |
| none |
true - input capture buffer is empty false - input capture buffer is not empty |
SCCP2_InputCapture_OverflowFlagClear()
void SCCP2_InputCapture_OverflowFlagClear (void )
Clears the buffer overflow status flag.
SCCP2_InputCapture_Initialize must be called |
| none |
none |
SCCP2_InputCapture_Start()
void SCCP2_InputCapture_Start (void )
Starts the InputCapture operation.
SCCP2_InputCapture_Initialize must be called |
| none |
none |
SCCP2_InputCapture_Stop()
void SCCP2_InputCapture_Stop (void )
Stops the InputCapture operation.
SCCP2_InputCapture_Initialize must be called |
| none |
none |
3.13.1.1.4 Variable Documentation
Input_Capture2
const struct INPUT_CAPTURE_INTERFACE Input_Capture2
Structure object of type INPUT_CAPTURE_INTERFACE with the custom name given by the user in the Melody Driver User interface. The default name e.g. Input_Capture1 can be changed by the user in the INPUT_CAPTURE user interface. This allows defining a structure with application specific name using the 'Custom Name' field. Application specific name allows the API Portability.
3.13.2 Data Structure Documentation
3.13.2.1 INPUT_CAPTURE_INTERFACE Struct Reference
Structure containing the function pointers of MCCP-InputCapture driver.
3.13.2.1.1 Detailed Description
Structure containing the function pointers of MCCP-InputCapture driver.
#include <input_capture_interface.h>
Data Fields
void(* Initialize )(void)
Pointer to SCCPx_InputCapture_Initialize e.g. SCCP1_InputCapture_Initialize.
void(* Deinitialize )(void)
Pointer to SCCPx_InputCapture_Deinitialize e.g. SCCP1_InputCapture_Deinitialize.
void(* Start )(void)
Pointer to SCCPx_InputCapture_Start e.g. SCCP1_InputCapture_Start.
void(* Stop )(void)
Pointer to SCCPx_InputCapture_Stop e.g. SCCP1_InputCapture_Stop.
void(* InputCapture_CallbackRegister )(void(*CallbackHandler)(void))
Pointer to SCCPx_InputCapture_CallbackRegister e.g. SCCP1_InputCapture_CallbackRegister.
void(* Tasks )(void)
Pointer to SCCPx_InputCapture_Tasks e.g. SCCP1_InputCapture_Tasks (Supported only in polling mode)
uint32_t(* DataRead )(void)
Pointer to SCCPx_InputCapture_DataRead e.g. SCCP1_InputCapture_DataRead.
bool(* HasBufferOverflowed )(void)
Pointer to SCCPx_InputCapture_HasBufferOverflowed e.g. SCCP1_InputCapture_HasBufferOverflowed.
bool(* IsBufferEmpty )(void)
Pointer to SCCPx_InputCapture_IsBufferEmpty e.g. SCCP1_InputCapture_IsBufferEmpty.
void(* OverflowFlagClear )(void)
Pointer to SCCPx_InputCapture_OverflowFlagClear e.g. SCCP1_InputCapture_OverflowFlagClear.
3.13.2.1.2 Field Documentation
The documentation for this struct was generated from the following file:
source/
DataRead
uint32_t(* DataRead) (void)
Pointer to SCCPx_InputCapture_DataRead e.g. SCCP1_InputCapture_DataRead.
Deinitialize
void(* Deinitialize) (void)
Pointer to SCCPx_InputCapture_Deinitialize e.g. SCCP1_InputCapture_Deinitialize.
HasBufferOverflowed
bool(* HasBufferOverflowed) (void)
Pointer to SCCPx_InputCapture_HasBufferOverflowed e.g. SCCP1_InputCapture_HasBufferOverflowed.
Initialize
void(* Initialize) (void)
Pointer to SCCPx_InputCapture_Initialize e.g. SCCP1_InputCapture_Initialize.
InputCapture_CallbackRegister
void(* InputCapture_CallbackRegister) (void(*CallbackHandler)(void))
Pointer to SCCPx_InputCapture_CallbackRegister e.g. SCCP1_InputCapture_CallbackRegister.
IsBufferEmpty
bool(* IsBufferEmpty) (void)
Pointer to SCCPx_InputCapture_IsBufferEmpty e.g. SCCP1_InputCapture_IsBufferEmpty.
OverflowFlagClear
void(* OverflowFlagClear) (void)
Pointer to SCCPx_InputCapture_OverflowFlagClear e.g. SCCP1_InputCapture_OverflowFlagClear.
Start
void(* Start) (void)
Pointer to SCCPx_InputCapture_Start e.g. SCCP1_InputCapture_Start.
Stop
void(* Stop) (void)
Pointer to SCCPx_InputCapture_Stop e.g. SCCP1_InputCapture_Stop.
Tasks
void(* Tasks) (void)
Pointer to SCCPx_InputCapture_Tasks e.g. SCCP1_InputCapture_Tasks (Supported only in polling mode)
3.13.3 File Documentation
3.13.3.1 source/input_capture_interface.h File Reference
#include <stdbool.h> #include <stdint.h>
3.13.3.1.1 Data structures
struct INPUT_CAPTURE_INTERFACE
Structure containing the function pointers of MCCP-InputCapture driver.
3.13.3.1.2 Detailed Description
MCCP-InputCapture Generated Driver Interface Header File
3.13.3.2 source/sccp2.h File Reference
#include <stdbool.h> #include <stdint.h> #include "input_capture_interface.h"
3.13.3.2.1 Functions
void SCCP2_InputCapture_Initialize (void)
Initializes the SCCP2-InputCapture module.
void SCCP2_InputCapture_Deinitialize (void)
Deinitializes the SCCP2-InputCapture to POR values.
void SCCP2_InputCapture_Start (void)
Starts the InputCapture operation.
void SCCP2_InputCapture_Stop (void)
Stops the InputCapture operation.
void SCCP2_InputCapture_CallbackRegister (void(*handler)(void))
This function can be used to override default callback and to define custom callback for SCCP2 InputCapture event.
void SCCP2_InputCapture_Callback (void)
This is the default callback with weak attribute. The user can override and implement the default callback without weak attribute or can register a custom callback function using SCCP2_InputCaptureCallbackRegister.
uint32_t SCCP2_InputCapture_DataRead (void)
Reads the captured value.
bool SCCP2_InputCapture_HasBufferOverflowed (void)
Returns the buffer overflow status.
bool SCCP2_InputCapture_IsBufferEmpty (void)
Returns the buffer empty status.
void SCCP2_InputCapture_OverflowFlagClear (void)
Clears the buffer overflow status flag.
3.13.3.2.2 Macros
#define SCCP2_CAPTURE_TIMER_FREQUENCY 4000000UL
This macro is used to read the Input Capture timer frequency (in Hz) for SCCP2 instance.
#define Input_Capture2_Initialize SCCP2_InputCapture_Initialize
This macro defines the Custom Name for SCCP2_InputCapture_Initialize API.
#define Input_Capture2_Deinitialize SCCP2_InputCapture_Deinitialize
This macro defines the Custom Name for SCCP2_InputCapture_Deinitialize API.
#define Input_Capture2_Start SCCP2_InputCapture_Start
This macro defines the Custom Name for SCCP2_InputCapture_Start API.
#define Input_Capture2_Stop SCCP2_InputCapture_Stop
This macro defines the Custom Name for SCCP2_InputCapture_Stop API.
#define Input_Capture2_Tasks SCCP2_InputCapture_Tasks
This macro defines the Custom Name for SCCP2_InputCapture_Tasks API.
#define Input_Capture2_DataRead SCCP2_InputCapture_DataRead
This macro defines the Custom Name for SCCP2_InputCapture_DataRead API.
#define Input_Capture2_HasBufferOverflowed SCCP2_InputCapture_HasBufferOverflowed
This macro defines the Custom Name for SCCP2_InputCapture_HasBufferOverflowed API.
#define Input_Capture2_IsBufferEmpty SCCP2_InputCapture_IsBufferEmpty
This macro defines the Custom Name for SCCP2_InputCapture_IsBufferEmpty API.
#define Input_Capture2_OverflowFlagClear SCCP2_InputCapture_OverflowFlagClear
This macro defines the Custom Name for SCCP2_InputCapture_OverflowFlagClear API.
#define Input_Capture2_InputCapture_CallbackRegister SCCP2_InputCapture_CallbackRegister
This macro defines the Custom Name for SCCP2_InputCapture_CallbackRegister API.
3.13.3.2.3 Variables
const struct INPUT_CAPTURE_INTERFACE Input_Capture2
Structure object of type INPUT_CAPTURE_INTERFACE with the custom name given by the user in the Melody Driver User interface. The default name e.g. Input_Capture1 can be changed by the user in the INPUT_CAPTURE user interface. This allows defining a structure with application specific name using the 'Custom Name' field. Application specific name allows the API Portability.
3.13.3.2.4 Macro Definition Documentation
SCCP2_CAPTURE_TIMER_FREQUENCY
#define SCCP2_CAPTURE_TIMER_FREQUENCY 4000000UL
This macro is used to read the Input Capture timer frequency (in Hz) for SCCP2 instance.