3.3 CBG Driver
Overview
The Current Bias Generator (CBG) consists of two classes of current sources:
- 10 uA Current Sources.
- Selectable Current Sources from 30-200 uA.
Features
- Simultaneous generation of 10uA and 50uA current source on dedicated output pins.
- Enabling 10uA and 50uA current sources enable the corresponding output pin as well.
3.3.1 Module Documentation
3.3.1.1 CBG Driver
Current Bias Generator driver is to configure 10uA and other selectable current sources using dsPIC MCUs.
3.3.1.1.1 Module description
Current Bias Generator driver is to configure 10uA and other selectable current sources using dsPIC MCUs.
Data structures
struct CBG_INTERFACE
Structure containing the function pointers of CBG driver.
Functions
void CBG_Initialize (void)
Initializes CBG module.
void CBG_Deinitialize (void)
Deinitializes the CBG to POR values.
Variables
const struct CBG_INTERFACE CBG
Structure object of type CBG_INTERFACE with the custom name given by the user in the Melody Driver User interface. The default name e.g. CBG can be changed by the user in the CBG user interface. This allows defining a structure with application specific name using the 'Custom Name' field. Application specific name allows the API Portability.
3.3.1.1.2 Function Documentation
CBG_Deinitialize()
void CBG_Deinitialize (void )
Deinitializes the CBG to POR values.
| none |
none |
CBG_Initialize()
void CBG_Initialize (void )
Initializes CBG module.
| none |
none |
3.3.1.1.3 Variable Documentation
CBG
const struct CBG_INTERFACE CBG
Structure object of type CBG_INTERFACE with the custom name given by the user in the Melody Driver User interface. The default name e.g. CBG can be changed by the user in the CBG user interface. This allows defining a structure with application specific name using the 'Custom Name' field. Application specific name allows the API Portability.
3.3.2 Data Structure Documentation
3.3.2.1 CBG_INTERFACE Struct Reference
Structure containing the function pointers of CBG driver.
3.3.2.1.1 Detailed Description
Structure containing the function pointers of CBG driver.
#include <cbg_interface.h>
Data Fields
void(* Initialize )(void)
Pointer to CBG_Initialize.
void(* Deinitialize )(void)
Pointer to CBG_Deinitialize.
3.3.2.1.2 Field Documentation
Deinitialize
void(* Deinitialize) (void)
Pointer to CBG_Deinitialize.
Initialize
void(* Initialize) (void)
Pointer to CBG_Initialize.
3.3.3 File Documentation
3.3.3.1 source/cbg.h File Reference
This is the generated driver header file for the CBG driver.
#include <xc.h> #include "cbg_interface.h"
3.3.3.1.1 Functions
void CBG_Initialize (void)
Initializes CBG module.
void CBG_Deinitialize (void)
Deinitializes the CBG to POR values.
3.3.3.1.2 Variables
const struct CBG_INTERFACE CBG
Structure object of type CBG_INTERFACE with the custom name given by the user in the Melody Driver User interface. The default name e.g. CBG can be changed by the user in the CBG user interface. This allows defining a structure with application specific name using the 'Custom Name' field. Application specific name allows the API Portability.
3.3.3.1.3 Detailed Description
This is the generated driver header file for the CBG driver.
CBG Generated Driver Header File
3.3.3.2 source/cbg_interface.h File Reference
3.3.3.2.1 Data structures
struct CBG_INTERFACE
Structure containing the function pointers of CBG driver.
3.3.3.2.2 Detailed Description
CBG Generated Driver Interface Header File