3.4 CMP DAC Driver
Overview
The high-speed analog comparator module provides a method to monitor voltage, current and other critical signals in a power conversion application that may be too fast for the CPU and ADC to capture.
The high-speed analog comparator module is comprised of a high-speed comparator, Pulse Density Modulation (PDM) DAC and a slope compensation unit. The slope compensation unit provides a user-defined slope which can be used to alter the DAC output. This feature is useful in applications, such as Peak Current mode control, where slope compensation is required to maintain the stability of the power supply
Features
- The user can configure the DAC Mode based on their application needs.
- There are four modes supported : DC-Mode, Slope Mode, Hysteretic Mode and Triangle Wave Mode.
- The Clock and Divider settings can be configured in the PLIB dependency of the driver module.
DAC Modes
DC-Mode

Slope Mode

Hysteretic Mode

Triangle Wave Mode

3.4.1 Module Documentation
3.4.1.1 CMP Driver
High Speed Analog Comparator with Slope Compensation DAC driver using dsPIC MCUs.
3.4.1.1.1 Module description
High Speed Analog Comparator with Slope Compensation DAC driver using dsPIC MCUs.
Data structures
struct DAC_DC_INTERFACE
Structure containing the function pointers of DAC driver in DC mode.
struct DAC_SLOPE_INTERFACE
Structure containing the function pointers of DAC driver in Slope mode.
struct CMP_INTERFACE
Structure containing the function pointers of CMP driver.
Definitions
#define CMP1_CLOCK_FREQUENCY 8000000UL
This macro defines input clock for CMP1.
#define CMP_DAC1_Initialize CMP1_Initialize
This macro defines the Custom Name for CMP1_Initialize API.
#define CMP_DAC1_Deinitialize CMP1_Deinitialize
This macro defines the Custom Name for CMP1_Deinitialize API.
#define CMP_DAC1_StatusGet CMP1_StatusGet
This macro defines the Custom Name for CMP1_StatusGet API.
#define CMP_DAC1_Enable CMP1_Enable
This macro defines the Custom Name for CMP1_Enable API.
#define CMP_DAC1_Disable CMP1_Disable
This macro defines the Custom Name for CMP1_Disable API.
#define CMP_DAC1_DACEnable CMP1_DACEnable
This macro defines the Custom Name for CMP1_DACEnable API.
#define CMP_DAC1_DACDisable CMP1_DACDisable
This macro defines the Custom Name for CMP1_DACDisable API.
#define CMP_DAC1_DACDataWrite CMP1_DACDataWrite
This macro defines the Custom Name for CMP1_DACDataWrite API.
#define CMP_DAC1_EventCallbackRegister CMP1_EventCallbackRegister
This macro defines the Custom Name for CMP1_EventCallbackRegister API.
#define CMP_DAC1_Tasks CMP1_Tasks
This macro defines the Custom Name for CMP1_Tasks API.
Functions
void CMP1_Initialize (void)
Initialize the CMP1 module.
void CMP1_Deinitialize (void)
Deinitializes the CMP1 to POR values.
void CMP1_Calibrate (void)
Calibrates the CMP1 module and enables ripple reduction mode.
static bool CMP1_StatusGet (void)
This inline function returns the comparator output status.
static void CMP1_Enable (void)
This inline function enables the common DAC module.
static void CMP1_Disable (void)
This inline function disables the common DAC module.
static void CMP1_DACEnable (void)
This inline function enables the individual DAC module.
static void CMP1_DACDisable (void)
This inline function disables the individual DAC module.
static void CMP1_DACDataWrite (size_t value)
This inline function writes DAC data to register.
void CMP1_EventCallbackRegister (void(*handler)(void))
This function can be used to override default callback and to define custom callback for CMP1 Event event.
void CMP1_EventCallback (void)
This is the default callback with weak attribute. The user can override and implement the default callback without weak attribute or can register a custom callback function using
CMP1_EventCallbackRegister.void CMP1_Tasks (void)
The Task function can be called in the main application using the High Speed Comparator, when interrupts are not used. This would thus introduce the polling mode feature of the Analog Comparator.
Variables
const struct CMP_INTERFACE CMP_DAC1
Structure object of type CMP_INTERFACE with the custom name given by the user in the Melody Driver User interface. The default name e.g. CMP_DAC1 can be changed by the user in the CMP user interface. This allows defining a structure with application specific name using the 'Custom Name' field. Application specific name allows the API Portability.
3.4.1.1.2 Definition Documentation
CMP1_CLOCK_FREQUENCY
#define CMP1_CLOCK_FREQUENCY 8000000UL
This macro defines input clock for CMP1.
CMP_DAC1_DACDataWrite
#define CMP_DAC1_DACDataWrite CMP1_DACDataWrite
This macro defines the Custom Name for CMP1_DACDataWrite API.
CMP_DAC1_DACDisable
#define CMP_DAC1_DACDisable CMP1_DACDisable
This macro defines the Custom Name for CMP1_DACDisable API.
CMP_DAC1_DACEnable
#define CMP_DAC1_DACEnable CMP1_DACEnable
This macro defines the Custom Name for CMP1_DACEnable API.
CMP_DAC1_Deinitialize
#define CMP_DAC1_Deinitialize CMP1_Deinitialize
This macro defines the Custom Name for CMP1_Deinitialize API.
CMP_DAC1_Disable
#define CMP_DAC1_Disable CMP1_Disable
This macro defines the Custom Name for CMP1_Disable API.
CMP_DAC1_Enable
#define CMP_DAC1_Enable CMP1_Enable
This macro defines the Custom Name for CMP1_Enable API.
CMP_DAC1_EventCallbackRegister
#define CMP_DAC1_EventCallbackRegister CMP1_EventCallbackRegister
This macro defines the Custom Name for CMP1_EventCallbackRegister API.
CMP_DAC1_Initialize
#define CMP_DAC1_Initialize CMP1_Initialize
This macro defines the Custom Name for CMP1_Initialize API.
CMP_DAC1_StatusGet
#define CMP_DAC1_StatusGet CMP1_StatusGet
This macro defines the Custom Name for CMP1_StatusGet API.
CMP_DAC1_Tasks
#define CMP_DAC1_Tasks CMP1_Tasks
This macro defines the Custom Name for CMP1_Tasks API.
3.4.1.1.3 Function Documentation
CMP1_Calibrate()
void CMP1_Calibrate (void )
Calibrates the CMP1 module and enables ripple reduction mode.
| none |
none |
CMP1_DACDataWrite()
inline static void CMP1_DACDataWrite (size_t value)
This inline function writes DAC data to register.
| in | value |
- DAC Data write value |
none |
CMP1_DACDisable()
inline static void CMP1_DACDisable (void )
This inline function disables the individual DAC module.
| none |
none |
CMP1_DACEnable()
inline static void CMP1_DACEnable (void )
This inline function enables the individual DAC module.
| none |
none |
CMP1_Deinitialize()
void CMP1_Deinitialize (void )
Deinitializes the CMP1 to POR values.
| none |
none |
CMP1_Disable()
inline static void CMP1_Disable (void )
This inline function disables the common DAC module.
| none |
none |
CMP1_Enable()
inline static void CMP1_Enable (void )
This inline function enables the common DAC module.
| none |
none |
CMP1_EventCallback()
void CMP1_EventCallback (void )
This is the default callback with weak attribute. The user can override and implement the default callback without weak attribute or can register a custom callback function using
CMP1_EventCallbackRegister.| none |
none |
CMP1_EventCallbackRegister()
void CMP1_EventCallbackRegister (void(*)(void) handler)
This function can be used to override default callback and to define custom callback for CMP1 Event event.
| in | handler |
- Address of the callback function. |
none |
CMP1_Initialize()
void CMP1_Initialize (void )
Initialize the CMP1 module.
| none |
none |
CMP1_StatusGet()
inline static bool CMP1_StatusGet (void )
This inline function returns the comparator output status.
| none |
true - Comparator output is high false - Comparator output is low |
CMP1_Tasks()
void CMP1_Tasks (void )
The Task function can be called in the main application using the High Speed Comparator, when interrupts are not used. This would thus introduce the polling mode feature of the Analog Comparator.
| none |
none |
3.4.1.1.4 Variable Documentation
CMP_DAC1
const struct CMP_INTERFACE CMP_DAC1
Structure object of type CMP_INTERFACE with the custom name given by the user in the Melody Driver User interface. The default name e.g. CMP_DAC1 can be changed by the user in the CMP user interface. This allows defining a structure with application specific name using the 'Custom Name' field. Application specific name allows the API Portability.
3.4.2 Data Structure Documentation
3.4.2.1 CMP_INTERFACE Struct Reference
Structure containing the function pointers of CMP driver.
3.4.2.1.1 Detailed Description
Structure containing the function pointers of CMP driver.
#include <cmp_interface.h>
Data Fields
void(* Initialize )(void)
Pointer to CMPx_Initialize e.g. CMP1_Initialize.
void(* Deinitialize )(void)
Pointer to CMPx_Deinitialize e.g. CMP1_Deinitialize.
void(* Calibrate )(void)
Pointer to CMPx_Deinitialize e.g. CMP1_Deinitialize.
void(* Enable )(void)
Pointer to CMPx_Enable e.g. CMP1_Enable.
void(* Disable )(void)
Pointer to CMPx_Disable e.g. CMP1_Disable.
bool(* StatusGet )(void)
Pointer to CMPx_StatusGet e.g. CMP1_StatusGet.
void(* EventCallbackRegister )(void(*handler)(void))
Pointer to CMPx_EventCallbackRegister e.g. CMP1_EventCallbackRegister.
void(* Tasks )(void)
Pointer to CMPx_Tasks e.g. CMP1_Tasks (Supported only in polling mode)
const struct DAC_DC_INTERFACE * cmp_dac_dc_interface
Pointer to DAC_DC_INTERFACE.
const struct DAC_SLOPE_INTERFACE * cmp_dac_slope_interface
Pointer to DAC_SLOPE_INTERFACE.
3.4.2.1.2 Field Documentation
Calibrate
void(* Calibrate) (void)
Pointer to CMPx_Deinitialize e.g. CMP1_Deinitialize.
cmp_dac_dc_interface
const struct DAC_DC_INTERFACE* cmp_dac_dc_interface
Pointer to DAC_DC_INTERFACE.
cmp_dac_slope_interface
const struct DAC_SLOPE_INTERFACE* cmp_dac_slope_interface
Pointer to DAC_SLOPE_INTERFACE.
Deinitialize
void(* Deinitialize) (void)
Pointer to CMPx_Deinitialize e.g. CMP1_Deinitialize.
Disable
void(* Disable) (void)
Pointer to CMPx_Disable e.g. CMP1_Disable.
Enable
void(* Enable) (void)
Pointer to CMPx_Enable e.g. CMP1_Enable.
EventCallbackRegister
void(* EventCallbackRegister) (void(*handler)(void))
Pointer to CMPx_EventCallbackRegister e.g. CMP1_EventCallbackRegister.
Initialize
void(* Initialize) (void)
Pointer to CMPx_Initialize e.g. CMP1_Initialize.
StatusGet
bool(* StatusGet) (void)
Pointer to CMPx_StatusGet e.g. CMP1_StatusGet.
Tasks
void(* Tasks) (void)
Pointer to CMPx_Tasks e.g. CMP1_Tasks (Supported only in polling mode)
3.4.2.2 DAC_DC_INTERFACE Struct Reference
Structure containing the function pointers of DAC driver in DC mode.
3.4.2.2.1 Detailed Description
Structure containing the function pointers of DAC driver in DC mode.
#include <cmp_interface.h>
Data Fields
void(* Enable )(void)
Pointer to CMPx_DACEnable e.g. CMP1_DACEnable.
void(* Disable )(void)
Pointer to CMPx_DACDisable e.g. CMP1_DACDisable.
void(* DataWrite )(size_t value)
Pointer to CMPx_DACDataWrite e.g. CMP1_DACDataWrite.
3.4.2.2.2 Field Documentation
DataWrite
void(* DataWrite) (size_t value)
Pointer to CMPx_DACDataWrite e.g. CMP1_DACDataWrite.
Disable
void(* Disable) (void)
Pointer to CMPx_DACDisable e.g. CMP1_DACDisable.
Enable
void(* Enable) (void)
Pointer to CMPx_DACEnable e.g. CMP1_DACEnable.
3.4.2.3 DAC_SLOPE_INTERFACE Struct Reference
Structure containing the function pointers of DAC driver in Slope mode.
3.4.2.3.1 Detailed Description
Structure containing the function pointers of DAC driver in Slope mode.
#include <cmp_interface.h>
Data Fields
void(* Enable )(void)
Pointer to CMPx_DACEnable e.g. CMP1_DACEnable.
void(* Disable )(void)
Pointer to CMPx_DACDisable e.g. CMP1_DACDisable.
void(* DataHighWrite )(uint16_t dacHighLimit)
Pointer to CMPx_DACDataHighWrite e.g. CMP1_DACDataHighWrite.
void(* DataLowWrite )(uint16_t dacLowLimit)
Pointer to CMPx_DACDataLowWrite e.g. CMP1_DACDataLowWrite.
void(* SlopeWrite )(uint16_t slopeRate)
Pointer to CMPx_DACSlopeWrite e.g. CMP1_DACSlopeWrite.
void(* SlopeUpdateMode )(enum CMP_DAC_SLOPE_UPDATE_MODE updateMode)
Pointer to CMPx_DACSlopeUpdateMode e.g. CMP1_DACSlopeUpdateMode.
3.4.2.3.2 Field Documentation
DataHighWrite
void(* DataHighWrite) (uint16_t dacHighLimit)
Pointer to CMPx_DACDataHighWrite e.g. CMP1_DACDataHighWrite.
DataLowWrite
void(* DataLowWrite) (uint16_t dacLowLimit)
Pointer to CMPx_DACDataLowWrite e.g. CMP1_DACDataLowWrite.
Disable
void(* Disable) (void)
Pointer to CMPx_DACDisable e.g. CMP1_DACDisable.
Enable
void(* Enable) (void)
Pointer to CMPx_DACEnable e.g. CMP1_DACEnable.
SlopeUpdateMode
void(* SlopeUpdateMode) (enum CMP_DAC_SLOPE_UPDATE_MODE updateMode)
Pointer to CMPx_DACSlopeUpdateMode e.g. CMP1_DACSlopeUpdateMode.
SlopeWrite
void(* SlopeWrite) (uint16_t slopeRate)
Pointer to CMPx_DACSlopeWrite e.g. CMP1_DACSlopeWrite.
3.4.3 File Documentation
3.4.3.1 source/cmp1.h File Reference
This is the generated driver header file for the CMP1 driver.
#include <stddef.h> #include <stdbool.h> #include <xc.h> #include "cmp_interface.h"
3.4.3.1.1 Functions
void CMP1_Initialize (void)
Initialize the CMP1 module.
void CMP1_Deinitialize (void)
Deinitializes the CMP1 to POR values.
void CMP1_Calibrate (void)
Calibrates the CMP1 module and enables ripple reduction mode.
static bool CMP1_StatusGet (void)
This inline function returns the comparator output status.
static void CMP1_Enable (void)
This inline function enables the common DAC module.
static void CMP1_Disable (void)
This inline function disables the common DAC module.
static void CMP1_DACEnable (void)
This inline function enables the individual DAC module.
static void CMP1_DACDisable (void)
This inline function disables the individual DAC module.
static void CMP1_DACDataWrite (size_t value)
This inline function writes DAC data to register.
void CMP1_EventCallbackRegister (void(*handler)(void))
This function can be used to override default callback and to define custom callback for CMP1 Event event.
void CMP1_EventCallback (void)
This is the default callback with weak attribute. The user can override and implement the default callback without weak attribute or can register a custom callback function using
CMP1_EventCallbackRegister.void CMP1_Tasks (void)
The Task function can be called in the main application using the High Speed Comparator, when interrupts are not used. This would thus introduce the polling mode feature of the Analog Comparator.
3.4.3.1.2 Macros
#define CMP1_CLOCK_FREQUENCY 8000000UL
This macro defines input clock for CMP1.
#define CMP_DAC1_Initialize CMP1_Initialize
This macro defines the Custom Name for CMP1_Initialize API.
#define CMP_DAC1_Deinitialize CMP1_Deinitialize
This macro defines the Custom Name for CMP1_Deinitialize API.
#define CMP_DAC1_StatusGet CMP1_StatusGet
This macro defines the Custom Name for CMP1_StatusGet API.
#define CMP_DAC1_Enable CMP1_Enable
This macro defines the Custom Name for CMP1_Enable API.
#define CMP_DAC1_Disable CMP1_Disable
This macro defines the Custom Name for CMP1_Disable API.
#define CMP_DAC1_DACEnable CMP1_DACEnable
This macro defines the Custom Name for CMP1_DACEnable API.
#define CMP_DAC1_DACDisable CMP1_DACDisable
This macro defines the Custom Name for CMP1_DACDisable API.
#define CMP_DAC1_DACDataWrite CMP1_DACDataWrite
This macro defines the Custom Name for CMP1_DACDataWrite API.
#define CMP_DAC1_EventCallbackRegister CMP1_EventCallbackRegister
This macro defines the Custom Name for CMP1_EventCallbackRegister API.
#define CMP_DAC1_Tasks CMP1_Tasks
This macro defines the Custom Name for CMP1_Tasks API.
3.4.3.1.3 Variables
const struct CMP_INTERFACE CMP_DAC1
Structure object of type CMP_INTERFACE with the custom name given by the user in the Melody Driver User interface. The default name e.g. CMP_DAC1 can be changed by the user in the CMP user interface. This allows defining a structure with application specific name using the 'Custom Name' field. Application specific name allows the API Portability.
3.4.3.1.4 Detailed Description
This is the generated driver header file for the CMP1 driver.
CMP1 Generated Driver Header File
3.4.3.2 source/cmp_interface.h File Reference
#include <stdbool.h> #include <stddef.h> #include <stdint.h> #include "cmp_types.h"
3.4.3.2.1 Data structures
struct DAC_DC_INTERFACE
Structure containing the function pointers of DAC driver in DC mode.
struct DAC_SLOPE_INTERFACE
Structure containing the function pointers of DAC driver in Slope mode.
struct CMP_INTERFACE
Structure containing the function pointers of CMP driver.
3.4.3.2.2 Detailed Description
CMP Generated Driver Interface Header File
3.4.3.3 source/cmp_types.h File Reference
This is the generated driver types header file for the CMP driver.
3.4.3.3.1 Enumerations
enum CMP_DAC_TRANSISION_MODE { CMP_DAC_TRANSISION_MODE_ENABLED = 0U, CMP_DAC_TRANSISION_MODE_DISABLED = 1U }
This enum is used to set the transision mode between smooth and slow transision or fast and sharp transision to new data values.
enum CMP_DAC_SLOPE_UPDATE_MODE { CMP_DAC_SLOPE_UPDATE_IMMIDIATE = 0U, CMP_DAC_SLOPE_UPDATE_TRIGGERED = 1U }
CMP slope data registers update mode.
3.4.3.3.2 Detailed Description
This is the generated driver types header file for the CMP driver.
CMP Generated Driver Types Header File
3.4.3.3.3 Enumeration Type Documentation
CMP_DAC_SLOPE_UPDATE_MODE
enum CMP_DAC_SLOPE_UPDATE_MODE
CMP slope data registers update mode.
Applicable in slope mode
| CMP_DAC_SLOPE_UPDATE_IMMIDIATE |
Updates slope related data registers immidiately |
| CMP_DAC_SLOPE_UPDATE_TRIGGERED |
Updates slope related data registers during the external trigger |
CMP_DAC_TRANSISION_MODE
enum CMP_DAC_TRANSISION_MODE
This enum is used to set the transision mode between smooth and slow transision or fast and sharp transision to new data values.
| CMP_DAC_TRANSISION_MODE_ENABLED |
Smoother and slower transision to the target value |
| CMP_DAC_TRANSISION_MODE_DISABLED |
Faster transision to the target value and ripple may be introduced |