3.15 Pulse Output Driver
Overview
Pulse Output Driver can be used to generate One shot Pulse or a series of output Pulses.Pulse Output Driver can be used to generate One shot Pulse or a series of output Pulses.
Features
- User configurable Pulse ON time.
- User configurable time interval between two consecutive Pulse to generate series of Output Pulses.
- Pulse ON time and Pulse interval time value range varies based on the clock source selected from Hardware Dependency module (PLIB).
-
Pulse Output depends on Synchronization (Sync) and Trigger source.
- In Sync operation, the Timer resets or clear occurs when the input selected by Sync is asserted.
- In Trigger operation, the Timer is held in reset until the input selected by Trigger is asserted.
The following waveform represents effect Sync source on Pulse generation.The following waveform represents effect Sync source on Pulse generation.
The following waveform represents effect Trigger source on Pulse generation.
3.15.1 Module Documentation
3.15.1.1 Event Output Driver
Event output Driver is used to generate single or series of Low, High or Toggle Output using dsPIC MCUs.
3.15.1.1.1 Module description
Event output Driver is used to generate single or series of Low, High or Toggle Output using dsPIC MCUs.
Data structures
struct EVENTOUTPUT_INTERFACE
Structure containing the function pointers of EVENTOUTPUT driver.
Definitions
#define Event_Output4_Initialize SCCP4_EventOutput_Initialize
This macro defines the Custom Name for SCCP4_EventOutput_Initialize API.
#define Event_Output4_Deinitialize SCCP4_EventOutput_Deinitialize
This macro defines the Custom Name for SCCP4_EventOutput_Deinitialize API.
#define Event_Output4_Enable SCCP4_EventOutput_Enable
This macro defines the Custom Name for SCCP4_EventOutput_Enable API.
#define Event_Output4_Disable SCCP4_EventOutput_Disable
This macro defines the Custom Name for SCCP4_EventOutput_Disable API.
#define Event_Output4_TransitTimeSet SCCP4_EventOutput_TransitTimeSet
This macro defines the Custom Name for SCCP4_EventOutput_TransitTimeSet API.
#define Event_Output4_SoftwareTriggerSet SCCP4_EventOutput_SoftwareTriggerSet
This macro defines the Custom Name for SCCP4_EventOutput_SoftwareTriggerSet API.
#define Event_Output4_EventOutput_CallbackRegister SCCP4_EventOutput_CallbackRegister
This macro defines the Custom Name for SCCP4_EventOutput_CallbackRegister API.
Functions
void SCCP4_EventOutput_Initialize (void)
Initializes the SCCP4 Edge Event driver. This function must be called before any other SCCP4 function is called.
void SCCP4_EventOutput_Deinitialize (void)
Deinitializes the SCCP4 to POR values.
void SCCP4_EventOutput_Enable (void)
Enables the SCCP4 module with the corresponding operation mode.
void SCCP4_EventOutput_Disable (void)
Disables the SCCP4 module.
void SCCP4_EventOutput_TransitTimeSet (uint32_t count)
Sets the compare values for SCCP4.
void SCCP4_EventOutput_SoftwareTriggerSet (void)
Sets the software trigger.
void SCCP4_EventOutput_CallbackRegister (void(*handler)(void))
This function can be used to override default callback and to define custom callback for SCCP4 EventOutput event.
void SCCP4_EventOutput_Callback (void)
This is the default callback with weak attribute. The user can override and implement the default callback without weak attribute or can register a custom callback function using SCCP4_EventOutput_CallbackRegister.
Variables
const struct EVENTOUTPUT_INTERFACE Event_Output4
Structure object of type EVENTOUTPUT_INTERFACE with the custom name given by the user in the Melody Driver User interface. The default name e.g. Event_Output1 can be changed by the user in the MCCP user interface. This allows defining a structure with application specific name using the 'Custom Name' field. Application specific name allows the API Portability.
3.15.1.1.2 Definition Documentation
Event_Output4_Deinitialize
#define Event_Output4_Deinitialize SCCP4_EventOutput_Deinitialize
This macro defines the Custom Name for SCCP4_EventOutput_Deinitialize API.
Event_Output4_Disable
#define Event_Output4_Disable SCCP4_EventOutput_Disable
This macro defines the Custom Name for SCCP4_EventOutput_Disable API.
Event_Output4_Enable
#define Event_Output4_Enable SCCP4_EventOutput_Enable
This macro defines the Custom Name for SCCP4_EventOutput_Enable API.
Event_Output4_EventOutput_CallbackRegister
#define Event_Output4_EventOutput_CallbackRegister SCCP4_EventOutput_CallbackRegister
This macro defines the Custom Name for SCCP4_EventOutput_CallbackRegister API.
Event_Output4_Initialize
#define Event_Output4_Initialize SCCP4_EventOutput_Initialize
This macro defines the Custom Name for SCCP4_EventOutput_Initialize API.
Event_Output4_SoftwareTriggerSet
#define Event_Output4_SoftwareTriggerSet SCCP4_EventOutput_SoftwareTriggerSet
This macro defines the Custom Name for SCCP4_EventOutput_SoftwareTriggerSet API.
Event_Output4_TransitTimeSet
#define Event_Output4_TransitTimeSet SCCP4_EventOutput_TransitTimeSet
This macro defines the Custom Name for SCCP4_EventOutput_TransitTimeSet API.
3.15.1.1.3 Function Documentation
SCCP4_EventOutput_Callback()
void SCCP4_EventOutput_Callback (void )
This is the default callback with weak attribute. The user can override and implement the default callback without weak attribute or can register a custom callback function using SCCP4_EventOutput_CallbackRegister.
| none |
none |
SCCP4_EventOutput_CallbackRegister()
void SCCP4_EventOutput_CallbackRegister (void(*)(void) handler)
This function can be used to override default callback and to define custom callback for SCCP4 EventOutput event.
| in | handler |
- Address of the callback function |
none |
SCCP4_EventOutput_Deinitialize()
void SCCP4_EventOutput_Deinitialize (void )
Deinitializes the SCCP4 to POR values.
| none |
none |
SCCP4_EventOutput_Disable()
void SCCP4_EventOutput_Disable (void )
Disables the SCCP4 module.
| none |
none |
SCCP4_EventOutput_Enable()
void SCCP4_EventOutput_Enable (void )
Enables the SCCP4 module with the corresponding operation mode.
| none |
none |
SCCP4_EventOutput_Initialize()
void SCCP4_EventOutput_Initialize (void )
Initializes the SCCP4 Edge Event driver. This function must be called before any other SCCP4 function is called.
| none |
none |
SCCP4_EventOutput_SoftwareTriggerSet()
void SCCP4_EventOutput_SoftwareTriggerSet (void )
Sets the software trigger.
| none |
none |
SCCP4_EventOutput_TransitTimeSet()
void SCCP4_EventOutput_TransitTimeSet (uint32_t count)
Sets the compare values for SCCP4.
| in | count |
- edge event wait time count |
none |
3.15.1.1.4 Variable Documentation
Event_Output4
const struct EVENTOUTPUT_INTERFACE Event_Output4
Structure object of type EVENTOUTPUT_INTERFACE with the custom name given by the user in the Melody Driver User interface. The default name e.g. Event_Output1 can be changed by the user in the MCCP user interface. This allows defining a structure with application specific name using the 'Custom Name' field. Application specific name allows the API Portability.
3.15.2 Data Structure Documentation
3.15.2.1 EVENTOUTPUT_INTERFACE Struct Reference
Structure containing the function pointers of EVENTOUTPUT driver.
3.15.2.1.1 Detailed Description
Structure containing the function pointers of EVENTOUTPUT driver.
#include <eventoutput_interface.h>
Data Fields
void(* Initialize )(void)
Pointer to SCCPx_EventOutput_Initialize e.g. SCCP1_EventOutput_Initialize.
void(* Deinitialize )(void)
Pointer to SCCPx_EventOutput_Deinitialize e.g. SCCP1_EventOutput_Deinitialize.
void(* Enable )(void)
Pointer to SCCPx_EventOutput_Enable e.g. SCCP1_EventOutput_Enable.
void(* Disable )(void)
Pointer to SCCPx_EventOutput_Disable e.g. SCCP1_EventOutput_Disable.
void(* TransitTimeSet )(uint32_t count)
Pointer to SCCPx_EventOutput_TransitTimeSet e.g. SCCP1_EventOutput_TransitTimeSet.
void(* SoftwareTriggerSet )(void)
Pointer to SCCPx_EventOutput_SoftwareTriggerSet e.g. SCCP1_EventOutput_SoftwareTriggerSet.
void(* CallbackRegister )(void(*handler)(void))
Pointer to SCCPx_EventOutput_CallbackRegister e.g. SCCP1_EventOutput_CallbackRegister.
void(* Tasks )(void)
Pointer to SCCPx_EventOutput_Tasks e.g. SCCP1_EventOutput_Tasks (Supported only in polling mode)
3.15.2.1.2 Field Documentation
The documentation for this struct was generated from the following file:
source/
CallbackRegister
void(* CallbackRegister) (void(*handler)(void))
Pointer to SCCPx_EventOutput_CallbackRegister e.g. SCCP1_EventOutput_CallbackRegister.
Deinitialize
void(* Deinitialize) (void)
Pointer to SCCPx_EventOutput_Deinitialize e.g. SCCP1_EventOutput_Deinitialize.
Disable
void(* Disable) (void)
Pointer to SCCPx_EventOutput_Disable e.g. SCCP1_EventOutput_Disable.
Enable
void(* Enable) (void)
Pointer to SCCPx_EventOutput_Enable e.g. SCCP1_EventOutput_Enable.
Initialize
void(* Initialize) (void)
Pointer to SCCPx_EventOutput_Initialize e.g. SCCP1_EventOutput_Initialize.
SoftwareTriggerSet
void(* SoftwareTriggerSet) (void)
Pointer to SCCPx_EventOutput_SoftwareTriggerSet e.g. SCCP1_EventOutput_SoftwareTriggerSet.
Tasks
void(* Tasks) (void)
Pointer to SCCPx_EventOutput_Tasks e.g. SCCP1_EventOutput_Tasks (Supported only in polling mode)
TransitTimeSet
void(* TransitTimeSet) (uint32_t count)
Pointer to SCCPx_EventOutput_TransitTimeSet e.g. SCCP1_EventOutput_TransitTimeSet.
3.15.3 File Documentation
3.15.3.1 source/eventoutput_interface.h File Reference
#include <stddef.h> #include <stdint.h>
3.15.3.1.1 Data structures
struct EVENTOUTPUT_INTERFACE
Structure containing the function pointers of EVENTOUTPUT driver.
3.15.3.1.2 Detailed Description
EVENTOUTPUT Generated Driver Interface Header File
3.15.3.2 source/sccp4.h File Reference
This is the generated driver header file for the SCCP4 driver.
#include <stddef.h> #include "eventoutput_interface.h"
3.15.3.2.1 Functions
void SCCP4_EventOutput_Initialize (void)
Initializes the SCCP4 Edge Event driver. This function must be called before any other SCCP4 function is called.
void SCCP4_EventOutput_Deinitialize (void)
Deinitializes the SCCP4 to POR values.
void SCCP4_EventOutput_Enable (void)
Enables the SCCP4 module with the corresponding operation mode.
void SCCP4_EventOutput_Disable (void)
Disables the SCCP4 module.
void SCCP4_EventOutput_TransitTimeSet (uint32_t count)
Sets the compare values for SCCP4.
void SCCP4_EventOutput_SoftwareTriggerSet (void)
Sets the software trigger.
void SCCP4_EventOutput_CallbackRegister (void(*handler)(void))
This function can be used to override default callback and to define custom callback for SCCP4 EventOutput event.
void SCCP4_EventOutput_Callback (void)
This is the default callback with weak attribute. The user can override and implement the default callback without weak attribute or can register a custom callback function using SCCP4_EventOutput_CallbackRegister.
3.15.3.2.2 Macros
#define Event_Output4_Initialize SCCP4_EventOutput_Initialize
This macro defines the Custom Name for SCCP4_EventOutput_Initialize API.
#define Event_Output4_Deinitialize SCCP4_EventOutput_Deinitialize
This macro defines the Custom Name for SCCP4_EventOutput_Deinitialize API.
#define Event_Output4_Enable SCCP4_EventOutput_Enable
This macro defines the Custom Name for SCCP4_EventOutput_Enable API.
#define Event_Output4_Disable SCCP4_EventOutput_Disable
This macro defines the Custom Name for SCCP4_EventOutput_Disable API.
#define Event_Output4_TransitTimeSet SCCP4_EventOutput_TransitTimeSet
This macro defines the Custom Name for SCCP4_EventOutput_TransitTimeSet API.
#define Event_Output4_SoftwareTriggerSet SCCP4_EventOutput_SoftwareTriggerSet
This macro defines the Custom Name for SCCP4_EventOutput_SoftwareTriggerSet API.
#define Event_Output4_EventOutput_CallbackRegister SCCP4_EventOutput_CallbackRegister
This macro defines the Custom Name for SCCP4_EventOutput_CallbackRegister API.
3.15.3.2.3 Variables
const struct EVENTOUTPUT_INTERFACE Event_Output4
Structure object of type EVENTOUTPUT_INTERFACE with the custom name given by the user in the Melody Driver User interface. The default name e.g. Event_Output1 can be changed by the user in the MCCP user interface. This allows defining a structure with application specific name using the 'Custom Name' field. Application specific name allows the API Portability.
3.15.3.2.4 Detailed Description
This is the generated driver header file for the SCCP4 driver.
SCCP4 Generated Driver Header File