3.10 Flash Driver
Overview
The Flash Driver helps the users to generate the Flash driver code. It provides the users easy to use Flash read, write and erase API's along with the required helper functions.
3.10.1 Module Documentation
3.10.1.1 Flash Driver
FLASH Driver using dsPIC MCUs.
3.10.1.1.1 Module description
FLASH Driver using dsPIC MCUs.
Data structures
struct FLASH_INTERFACE
Structure containing the function pointers of FLASH driver.
Definitions
#define FLASH_ADDRESS_MASK 4U
Defines FLASH odd address mask value.
#define FLASH_UNLOCK_KEY 0x00AA0055
Defines FLASH unlock key.
#define FLASH_PAGE_ERASE_OPCODE 0x4003
Defines FLASH page erase opcode.
#define FLASH_WORD_WRITE_OPCODE 0x4001
Defines FLASH word write opcode.
#define FLASH_ROW_WRITE_OPCODE 0x4002
Defines FLASH word write opcode.
#define FLASH_ERASE_PAGE_SIZE_IN_INSTRUCTIONS 512U
Defines FLASH flash page size.
#define FLASH_ERASE_PAGE_MASK (~(FLASH_ERASE_PAGE_SIZE_IN_INSTRUCTIONS - 1U))
Defines FLASH erase page mask.
Enumerations
enum FLASH_PANEL { FLASH_PANEL_1 = 0, FLASH_PANEL_2 = 1, FLASH_PANEL_MAX_PANELS }
This enum is be used for the flash panel numbers and maximum flash panels.
enum FLASH_RETURN_STATUS { FLASH_NO_ERROR, FLASH_INVALID_ADDRESS, FLASH_INVALID_DATA, FLASH_WRITE_ERROR, FLASH_READ_ERROR, FLASH_ERASE_ERROR, FLASH_INVALID_CALLBACK_HANDLER, FLASH_OP_BUSY, FLASH_OP_IN_PROGRESS, FLASH_INVALID_KEY, FLASH_INVALID_OEPRATION, FLASH_SECURITY_ACCESS_CONTROL_ERROR, FLASH_PANEL_CONTROL_LOGIC_ERROR, FLASH_ROW_OP_SYSTEM_BUS_ERROR, FLASH_ROW_OP_WARM_RESET_ERROR }
This enum is be used to return the status of write, read and erase operation.
Functions
enum FLASH_RETURN_STATUS FLASH_PageErase (flash_adr_t flashAddress, flash_key_t unlockKey)
This function erases a page.
enum FLASH_RETURN_STATUS FLASH_WordWrite (flash_adr_t flashAddress, flash_data_t *data, flash_key_t unlockKey)
This function writes the specified data to the specified address.
enum FLASH_RETURN_STATUS FLASH_RowWrite (flash_adr_t flashAddress, flash_data_t *data, flash_key_t unlockKey)
This function writes the specified data to the specified address.
enum FLASH_RETURN_STATUS FLASH_Read (flash_adr_t flashAddress, size_t count, flash_data_t *data)
This function reads the data from the specified address.
uint16_t FLASH_ErasePageOffsetGet (flash_adr_t flashAddress)
This function returns the offest from page start.
uint32_t FLASH_ErasePageAddressGet (flash_adr_t flashAddress)
This function returns the offest from page start.
Variables
const struct FLASH_INTERFACE flash
Structure object of type FLASH_INTERFACE assigned with name displayed in the Melody Driver User interface. A structure pointer can be used to achieve portability across the FLASH having same interface structure.
3.10.1.1.2 Definition Documentation
FLASH_ADDRESS_MASK
#define FLASH_ADDRESS_MASK 4U
Defines FLASH odd address mask value.
FLASH_ERASE_PAGE_MASK
#define FLASH_ERASE_PAGE_MASK (~(FLASH_ERASE_PAGE_SIZE_IN_INSTRUCTIONS - 1U))
Defines FLASH erase page mask.
FLASH_ERASE_PAGE_SIZE_IN_INSTRUCTIONS
#define FLASH_ERASE_PAGE_SIZE_IN_INSTRUCTIONS 512U
Defines FLASH flash page size.
FLASH_PAGE_ERASE_OPCODE
#define FLASH_PAGE_ERASE_OPCODE 0x4003
Defines FLASH page erase opcode.
FLASH_ROW_WRITE_OPCODE
#define FLASH_ROW_WRITE_OPCODE 0x4002
Defines FLASH word write opcode.
FLASH_UNLOCK_KEY
#define FLASH_UNLOCK_KEY 0x00AA0055
Defines FLASH unlock key.
FLASH_WORD_WRITE_OPCODE
#define FLASH_WORD_WRITE_OPCODE 0x4001
Defines FLASH word write opcode.
3.10.1.1.3 Function Documentation
FLASH_ErasePageAddressGet()
uint32_t FLASH_ErasePageAddressGet (flash_adr_t flashAddress)
This function returns the offest from page start.
| in | flashAddress |
: Flash address |
FLASH_RETURN_STATUS: returns page start address for the given address |
FLASH_ErasePageOffsetGet()
uint16_t FLASH_ErasePageOffsetGet (flash_adr_t flashAddress)
This function returns the offest from page start.
| in | flashAddress |
: Flash address |
FLASH_RETURN_STATUS: returns the flash offset from page start address |
FLASH_PageErase()
enum FLASH_RETURN_STATUS FLASH_PageErase (flash_adr_t flashAddress, flash_key_t unlockKey)
This function erases a page.
| in | flashAddress |
: Flash address |
| in | unlockKey |
: Pointer of the data to be written |
FLASH_RETURN_STATUS: returns FLASH_NO_ERROR if operation is successful , else returns errors like FLASH_INVALID_ADDRESS, FLASH_WRITE_ERROR |
FLASH_Read()
enum FLASH_RETURN_STATUS FLASH_Read (flash_adr_t flashAddress, size_t count, flash_data_t * data)
This function reads the data from the specified address.
| in | flashAddress |
: Flash address |
| out | data |
: Pointer to read the data |
FLASH_RETURN_STATUS: returns FLASH_NO_ERROR if operation is successful , else returns errors like FLASH_INVALID_ADDRESS, FLASH_INVALID_DATA |
FLASH_RowWrite()
enum FLASH_RETURN_STATUS FLASH_RowWrite (flash_adr_t flashAddress, flash_data_t * data, flash_key_t unlockKey)
This function writes the specified data to the specified address.
| in | flashAddress |
: Flash address |
| in | data |
: Pointer of the data to be written |
FLASH_RETURN_STATUS: returns FLASH_NO_ERROR if operation is successful , else returns errors like FLASH_INVALID_ADDRESS, FLASH_INVALID_DATA, FLASH_WRITE_ERROR |
FLASH_WordWrite()
enum FLASH_RETURN_STATUS FLASH_WordWrite (flash_adr_t flashAddress, flash_data_t * data, flash_key_t unlockKey)
This function writes the specified data to the specified address.
| in | flashAddress |
: Flash address |
| in | data |
: Pointer of the data to be written. This will write the 4 WORDS pointed to by the pointer. |
FLASH_RETURN_STATUS: returns FLASH_NO_ERROR if operation is successful , else returns errors like FLASH_INVALID_ADDRESS, FLASH_INVALID_DATA, FLASH_WRITE_ERROR |
3.10.1.1.4 Enumeration Type Documentation
FLASH_PANEL
enum FLASH_PANEL
This enum is be used for the flash panel numbers and maximum flash panels.
| FLASH_PANEL_1 | |
| FLASH_PANEL_2 | |
| FLASH_PANEL_MAX_PANELS |
FLASH_RETURN_STATUS
enum FLASH_RETURN_STATUS
This enum is be used to return the status of write, read and erase operation.
| FLASH_NO_ERROR |
No error occurred |
| FLASH_INVALID_ADDRESS |
Invalid address |
| FLASH_INVALID_DATA |
Invalid data |
| FLASH_WRITE_ERROR |
Write error has occurred |
| FLASH_READ_ERROR |
Read error has occurred |
| FLASH_ERASE_ERROR |
Flash erase error occurred |
| FLASH_INVALID_CALLBACK_HANDLER |
Invalid parameter to operation |
| FLASH_OP_BUSY |
Flash is physically busy |
| FLASH_OP_IN_PROGRESS |
Flash operation is in progress |
| FLASH_INVALID_KEY |
Invalid NVM unlock Key |
| FLASH_INVALID_OEPRATION |
Invalid program/erase operation (PROGOP) |
| FLASH_SECURITY_ACCESS_CONTROL_ERROR |
Flash Security access control violation |
| FLASH_PANEL_CONTROL_LOGIC_ERROR |
Error reported by flash panel control logic |
| FLASH_ROW_OP_SYSTEM_BUS_ERROR |
Flash System bus error during row operation |
| FLASH_ROW_OP_WARM_RESET_ERROR |
Row programming operation not completed due to warm reset |
3.10.1.1.5 Variable Documentation
flash
const struct FLASH_INTERFACE flash
Structure object of type FLASH_INTERFACE assigned with name displayed in the Melody Driver User interface. A structure pointer can be used to achieve portability across the FLASH having same interface structure.
3.10.2 Data Structure Documentation
3.10.2.1 FLASH_INTERFACE Struct Reference
Structure containing the function pointers of FLASH driver.
3.10.2.1.1 Detailed Description
Structure containing the function pointers of FLASH driver.
#include <flash_interface.h>
Data Fields
enum FLASH_RETURN_STATUS(* PageErase )(flash_adr_t address, flash_key_t unlockKey)
Pointer to FLASH_PageErase e.g. FLASH_PageErase.
enum FLASH_RETURN_STATUS(* Write )(flash_adr_t address, flash_data_t *data, flash_key_t unlockKey)
Pointer to FLASH_WordWrite e.g. FLASH_WordWrite.
enum FLASH_RETURN_STATUS(* RowWrite )(flash_adr_t address, flash_data_t *data, flash_key_t unlockKey)
Pointer to FLASH_RowWrite e.g. FLASH_RowWrite.
enum FLASH_RETURN_STATUS(* Read )(flash_adr_t address, size_t count, uint32_t *data)
Pointer to FLASH_Read e.g. FLASH_Read.
uint32_t(* PageAddressGet )(flash_adr_t address)
Pointer to FLASH_ErasePageAddressGet e.g. FLASH_ErasePageAddressGet.
uint16_t(* PageOffsetGet )(flash_adr_t address)
Pointer to FLASH_ErasePageOffsetGet e.g. FLASH_ErasePageOffsetGet.
enum FLASH_RETURN_STATUS(* OperationStatusGet )(void)
Pointer to FLASH_OperationStatusGet e.g. FLASH_OperationStatusGet.
enum FLASH_RETURN_STATUS(* NonBlockingPageErase )(flash_adr_t address, flash_key_t unlockKey, FLASH_CALLBACK callbackHandler, void *context)
Pointer to FLASH_NonBlockingPageErase e.g. FLASH_NonBlockingPageErase.
enum FLASH_RETURN_STATUS(* NonBlockingBulkErase )(enum FLASH_PANEL panel, flash_key_t unlockKey, FLASH_CALLBACK callbackHandler, void *context)
Pointer to FLASH_NonBlockingBulkErase e.g. FLASH_NonBlockingBulkErase.
enum FLASH_RETURN_STATUS(* NonBlockingWordWrite )(flash_adr_t address, flash_data_t *data, flash_key_t unlockKey, FLASH_CALLBACK callbackHandler, void *context)
Pointer to FLASH_NonBlockingWordWrite e.g. FLASH_NonBlockingWordWrite.
enum FLASH_RETURN_STATUS(* NonBlockingRowWrite )(flash_adr_t address, flash_data_t *data, flash_key_t unlockKey, FLASH_CALLBACK callbackHandler, void *context)
Pointer to FLASH_NonBlockingRowWrite e.g. FLASH_NonBlockingRowWrite.
enum FLASH_RETURN_STATUS(* NonBlockingRead )(flash_adr_t address, size_t count, uint32_t *data)
Pointer to FLASH_NonBlockingRead e.g. FLASH_NonBlockingRead.
enum FLASH_RETURN_STATUS(* NonBlockingPolledPageErase )(flash_adr_t address, flash_key_t unlockKey)
Pointer to FLASH_NonBlockingPolledPageErase e.g. FLASH_NonBlockingPolledPageErase.
enum FLASH_RETURN_STATUS(* NonBlockingPolledBulkErase )(enum FLASH_PANEL panel, flash_key_t unlockKey)
Pointer to FLASH_NonBlockingPolledBulkErase e.g. FLASH_NonBlockingPolledBulkErase.
enum FLASH_RETURN_STATUS(* NonBlockingPolledWordWrite )(flash_adr_t address, flash_data_t *data, flash_key_t unlockKey)
Pointer to FLASH_NonBlockingPolledWordWrite e.g. FLASH_NonBlockingPolledWordWrite.
enum FLASH_RETURN_STATUS(* NonBlockingPolledRowWrite )(flash_adr_t address, flash_data_t *data, flash_key_t unlockKey)
Pointer to FLASH_NonBlockingPolledRowWrite e.g. FLASH_NonBlockingPolledRowWrite.
enum FLASH_RETURN_STATUS(* NonBlockingPolledRead )(flash_adr_t address, size_t count, uint32_t *data)
Pointer to FLASH_NonBlockingPolledRead e.g. FLASH_NonBlockingPolledRead.
3.10.2.1.2 Field Documentation
NonBlockingBulkErase
enum FLASH_RETURN_STATUS(* NonBlockingBulkErase) (enum FLASH_PANEL panel, flash_key_t unlockKey, FLASH_CALLBACK callbackHandler, void *context)
Pointer to FLASH_NonBlockingBulkErase e.g. FLASH_NonBlockingBulkErase.
NonBlockingPageErase
enum FLASH_RETURN_STATUS(* NonBlockingPageErase) (flash_adr_t address, flash_key_t unlockKey, FLASH_CALLBACK callbackHandler, void *context)
Pointer to FLASH_NonBlockingPageErase e.g. FLASH_NonBlockingPageErase.
NonBlockingPolledBulkErase
enum FLASH_RETURN_STATUS(* NonBlockingPolledBulkErase) (enum FLASH_PANEL panel, flash_key_t unlockKey)
Pointer to FLASH_NonBlockingPolledBulkErase e.g. FLASH_NonBlockingPolledBulkErase.
NonBlockingPolledPageErase
enum FLASH_RETURN_STATUS(* NonBlockingPolledPageErase) (flash_adr_t address, flash_key_t unlockKey)
Pointer to FLASH_NonBlockingPolledPageErase e.g. FLASH_NonBlockingPolledPageErase.
NonBlockingPolledRead
enum FLASH_RETURN_STATUS(* NonBlockingPolledRead) (flash_adr_t address, size_t count, uint32_t *data)
Pointer to FLASH_NonBlockingPolledRead e.g. FLASH_NonBlockingPolledRead.
NonBlockingPolledRowWrite
enum FLASH_RETURN_STATUS(* NonBlockingPolledRowWrite) (flash_adr_t address, flash_data_t *data, flash_key_t unlockKey)
Pointer to FLASH_NonBlockingPolledRowWrite e.g. FLASH_NonBlockingPolledRowWrite.
NonBlockingPolledWordWrite
enum FLASH_RETURN_STATUS(* NonBlockingPolledWordWrite) (flash_adr_t address, flash_data_t *data, flash_key_t unlockKey)
Pointer to FLASH_NonBlockingPolledWordWrite e.g. FLASH_NonBlockingPolledWordWrite.
NonBlockingRead
enum FLASH_RETURN_STATUS(* NonBlockingRead) (flash_adr_t address, size_t count, uint32_t *data)
Pointer to FLASH_NonBlockingRead e.g. FLASH_NonBlockingRead.
NonBlockingRowWrite
enum FLASH_RETURN_STATUS(* NonBlockingRowWrite) (flash_adr_t address, flash_data_t *data, flash_key_t unlockKey, FLASH_CALLBACK callbackHandler, void *context)
Pointer to FLASH_NonBlockingRowWrite e.g. FLASH_NonBlockingRowWrite.
NonBlockingWordWrite
enum FLASH_RETURN_STATUS(* NonBlockingWordWrite) (flash_adr_t address, flash_data_t *data, flash_key_t unlockKey, FLASH_CALLBACK callbackHandler, void *context)
Pointer to FLASH_NonBlockingWordWrite e.g. FLASH_NonBlockingWordWrite.
OperationStatusGet
enum FLASH_RETURN_STATUS(* OperationStatusGet) (void)
Pointer to FLASH_OperationStatusGet e.g. FLASH_OperationStatusGet.
PageAddressGet
uint32_t(* PageAddressGet) (flash_adr_t address)
Pointer to FLASH_ErasePageAddressGet e.g. FLASH_ErasePageAddressGet.
PageErase
enum FLASH_RETURN_STATUS(* PageErase) (flash_adr_t address, flash_key_t unlockKey)
Pointer to FLASH_PageErase e.g. FLASH_PageErase.
PageOffsetGet
uint16_t(* PageOffsetGet) (flash_adr_t address)
Pointer to FLASH_ErasePageOffsetGet e.g. FLASH_ErasePageOffsetGet.
Read
enum FLASH_RETURN_STATUS(* Read) (flash_adr_t address, size_t count, uint32_t *data)
Pointer to FLASH_Read e.g. FLASH_Read.
RowWrite
enum FLASH_RETURN_STATUS(* RowWrite) (flash_adr_t address, flash_data_t *data, flash_key_t unlockKey)
Pointer to FLASH_RowWrite e.g. FLASH_RowWrite.
Write
enum FLASH_RETURN_STATUS(* Write) (flash_adr_t address, flash_data_t *data, flash_key_t unlockKey)
Pointer to FLASH_WordWrite e.g. FLASH_WordWrite.
3.10.3 File Documentation
3.10.3.1 source/flash.h File Reference
FLASH driver using dsPIC MCUs.
#include <stdint.h> #include <stddef.h> #include <stdbool.h> #include "flash_interface.h"
3.10.3.1.1 Functions
enum FLASH_RETURN_STATUS FLASH_PageErase (flash_adr_t flashAddress, flash_key_t unlockKey)
This function erases a page.
enum FLASH_RETURN_STATUS FLASH_WordWrite (flash_adr_t flashAddress, flash_data_t *data, flash_key_t unlockKey)
This function writes the specified data to the specified address.
enum FLASH_RETURN_STATUS FLASH_RowWrite (flash_adr_t flashAddress, flash_data_t *data, flash_key_t unlockKey)
This function writes the specified data to the specified address.
enum FLASH_RETURN_STATUS FLASH_Read (flash_adr_t flashAddress, size_t count, flash_data_t *data)
This function reads the data from the specified address.
uint16_t FLASH_ErasePageOffsetGet (flash_adr_t flashAddress)
This function returns the offest from page start.
uint32_t FLASH_ErasePageAddressGet (flash_adr_t flashAddress)
This function returns the offest from page start.
3.10.3.1.2 Variables
const struct FLASH_INTERFACE flash
Structure object of type FLASH_INTERFACE assigned with name displayed in the Melody Driver User interface. A structure pointer can be used to achieve portability across the FLASH having same interface structure.
3.10.3.1.3 Detailed Description
FLASH driver using dsPIC MCUs.
FLASH Generated Driver Header File
3.10.3.2 source/flash_interface.h File Reference
#include <stdint.h> #include <stdbool.h> #include <stddef.h> #include "flash_types.h"
3.10.3.2.1 Data structures
struct FLASH_INTERFACE
Structure containing the function pointers of FLASH driver.
3.10.3.2.2 Detailed Description
flash Generated Driver Interface Header File
3.10.3.3 source/flash_types.h File Reference
FLASH Driver using dsPIC MCUs.
3.10.3.3.1 Macros
#define FLASH_ADDRESS_MASK 4U
Defines FLASH odd address mask value.
#define FLASH_UNLOCK_KEY 0x00AA0055
Defines FLASH unlock key.
#define FLASH_PAGE_ERASE_OPCODE 0x4003
Defines FLASH page erase opcode.
#define FLASH_WORD_WRITE_OPCODE 0x4001
Defines FLASH word write opcode.
#define FLASH_ROW_WRITE_OPCODE 0x4002
Defines FLASH word write opcode.
#define FLASH_ERASE_PAGE_SIZE_IN_INSTRUCTIONS 512U
Defines FLASH flash page size.
#define FLASH_ERASE_PAGE_MASK (~(FLASH_ERASE_PAGE_SIZE_IN_INSTRUCTIONS - 1U))
Defines FLASH erase page mask.
3.10.3.3.2 Typedefs
typedef void(* FLASH_CALLBACK) (void *)
typedef uint32_t flash_adr_t
typedef uint32_t flash_data_t
typedef uint32_t flash_key_t
3.10.3.3.3 Enumerations
enum FLASH_PANEL { FLASH_PANEL_1 = 0, FLASH_PANEL_2 = 1, FLASH_PANEL_MAX_PANELS }
This enum is be used for the flash panel numbers and maximum flash panels.
enum FLASH_RETURN_STATUS { FLASH_NO_ERROR, FLASH_INVALID_ADDRESS, FLASH_INVALID_DATA, FLASH_WRITE_ERROR, FLASH_READ_ERROR, FLASH_ERASE_ERROR, FLASH_INVALID_CALLBACK_HANDLER, FLASH_OP_BUSY, FLASH_OP_IN_PROGRESS, FLASH_INVALID_KEY, FLASH_INVALID_OEPRATION, FLASH_SECURITY_ACCESS_CONTROL_ERROR, FLASH_PANEL_CONTROL_LOGIC_ERROR, FLASH_ROW_OP_SYSTEM_BUS_ERROR, FLASH_ROW_OP_WARM_RESET_ERROR }
This enum is be used to return the status of write, read and erase operation.
3.10.3.3.4 Detailed Description
FLASH Driver using dsPIC MCUs.
flash Generated Driver Types Header File
3.10.3.3.5 Typedef Documentation
flash_adr_t
typedef uint32_t flash_adr_t
FLASH_CALLBACK
typedef void(* FLASH_CALLBACK) (void *)
flash_data_t
typedef uint32_t flash_data_t
flash_key_t
typedef uint32_t flash_key_t