3.29.5 Pins Driver
Overview
The Pins Driver provides the Firmware Implementations of Device pins used by the Peripherals.
Features
Based on the Pin Configuration in MCC Melody User interface Pin specific registers are generated as listed below
- GPIO Pin APIs
- IOC - Interrupt-on-Change Registers and APIs
-
PPS - Peripheral Pin Select Module Registers
- Input
- Output
- Bi-Directional
-
I/O Ports Registers
- PORTx - Port Register
- LATx - Latch Register
- TRISx - Direction Register
- ANSELx - Analog Register
- CNPUx - Weak-Pull Up
- CNPDx - Weak-Pull Down
- ODCx - Output Drain
3.29.5.1 Module Documentation
3.29.5.1.1 Pins Driver
The Pin Driver directs the operation and function of the selected device pins using dsPIC MCUs.
Module description
The Pin Driver directs the operation and function of the selected device pins using dsPIC MCUs.
Definitions
#define IO_RA5_SetHigh() (_LATA5 = 1)
Sets the RA5 GPIO Pin which has a custom name of IO_RA5 to High.
#define IO_RA5_SetLow() (_LATA5 = 0)
Sets the RA5 GPIO Pin which has a custom name of IO_RA5 to Low.
#define IO_RA5_Toggle() (_LATA5 ^= 1)
Toggles the RA5 GPIO Pin which has a custom name of IO_RA5.
#define IO_RA5_GetValue() _RA5
Reads the value of the RA5 GPIO Pin which has a custom name of IO_RA5.
#define IO_RA5_SetDigitalInput() (_TRISA5 = 1)
Configures the RA5 GPIO Pin which has a custom name of IO_RA5 as Input.
#define IO_RA5_SetDigitalOutput() (_TRISA5 = 0)
Configures the RA5 GPIO Pin which has a custom name of IO_RA5 as Output.
#define IO_RA8_SetHigh() (_LATA8 = 1)
Sets the RA8 GPIO Pin which has a custom name of IO_RA8 to High.
#define IO_RA8_SetLow() (_LATA8 = 0)
Sets the RA8 GPIO Pin which has a custom name of IO_RA8 to Low.
#define IO_RA8_Toggle() (_LATA8 ^= 1)
Toggles the RA8 GPIO Pin which has a custom name of IO_RA8.
#define IO_RA8_GetValue() _RA8
Reads the value of the RA8 GPIO Pin which has a custom name of IO_RA8.
#define IO_RA8_SetDigitalInput() (_TRISA8 = 1)
Configures the RA8 GPIO Pin which has a custom name of IO_RA8 as Input.
#define IO_RA8_SetDigitalOutput() (_TRISA8 = 0)
Configures the RA8 GPIO Pin which has a custom name of IO_RA8 as Output.
#define IO_RA11_SetHigh() (_LATA11 = 1)
Sets the RA11 GPIO Pin which has a custom name of IO_RA11 to High.
#define IO_RA11_SetLow() (_LATA11 = 0)
Sets the RA11 GPIO Pin which has a custom name of IO_RA11 to Low.
#define IO_RA11_Toggle() (_LATA11 ^= 1)
Toggles the RA11 GPIO Pin which has a custom name of IO_RA11.
#define IO_RA11_GetValue() _RA11
Reads the value of the RA11 GPIO Pin which has a custom name of IO_RA11.
#define IO_RA11_SetDigitalInput() (_TRISA11 = 1)
Configures the RA11 GPIO Pin which has a custom name of IO_RA11 as Input.
#define IO_RA11_SetDigitalOutput() (_TRISA11 = 0)
Configures the RA11 GPIO Pin which has a custom name of IO_RA11 as Output.
Functions
void PINS_Initialize (void)
Initializes the PINS module.
Definition Documentation
IO_RA11_GetValue
#define IO_RA11_GetValue( ) _RA11
Reads the value of the RA11 GPIO Pin which has a custom name of IO_RA11.
| none |
none |
IO_RA11_SetDigitalInput
#define IO_RA11_SetDigitalInput( ) (_TRISA11 = 1)
Configures the RA11 GPIO Pin which has a custom name of IO_RA11 as Input.
| none |
none |
IO_RA11_SetDigitalOutput
#define IO_RA11_SetDigitalOutput( ) (_TRISA11 = 0)
Configures the RA11 GPIO Pin which has a custom name of IO_RA11 as Output.
| none |
none |
IO_RA11_SetHigh
#define IO_RA11_SetHigh( ) (_LATA11 = 1)
Sets the RA11 GPIO Pin which has a custom name of IO_RA11 to High.
The RA11 must be set as Output Pin |
| none |
none |
IO_RA11_SetLow
#define IO_RA11_SetLow( ) (_LATA11 = 0)
Sets the RA11 GPIO Pin which has a custom name of IO_RA11 to Low.
The RA11 must be set as Output Pin |
| none |
none |
IO_RA11_Toggle
#define IO_RA11_Toggle( ) (_LATA11 ^= 1)
Toggles the RA11 GPIO Pin which has a custom name of IO_RA11.
The RA11 must be set as Output Pin |
| none |
none |
IO_RA5_GetValue
#define IO_RA5_GetValue( ) _RA5
Reads the value of the RA5 GPIO Pin which has a custom name of IO_RA5.
| none |
none |
IO_RA5_SetDigitalInput
#define IO_RA5_SetDigitalInput( ) (_TRISA5 = 1)
Configures the RA5 GPIO Pin which has a custom name of IO_RA5 as Input.
| none |
none |
IO_RA5_SetDigitalOutput
#define IO_RA5_SetDigitalOutput( ) (_TRISA5 = 0)
Configures the RA5 GPIO Pin which has a custom name of IO_RA5 as Output.
| none |
none |
IO_RA5_SetHigh
#define IO_RA5_SetHigh( ) (_LATA5 = 1)
Sets the RA5 GPIO Pin which has a custom name of IO_RA5 to High.
The RA5 must be set as Output Pin |
| none |
none |
IO_RA5_SetLow
#define IO_RA5_SetLow( ) (_LATA5 = 0)
Sets the RA5 GPIO Pin which has a custom name of IO_RA5 to Low.
The RA5 must be set as Output Pin |
| none |
none |
IO_RA5_Toggle
#define IO_RA5_Toggle( ) (_LATA5 ^= 1)
Toggles the RA5 GPIO Pin which has a custom name of IO_RA5.
The RA5 must be set as Output Pin |
| none |
none |
IO_RA8_GetValue
#define IO_RA8_GetValue( ) _RA8
Reads the value of the RA8 GPIO Pin which has a custom name of IO_RA8.
| none |
none |
IO_RA8_SetDigitalInput
#define IO_RA8_SetDigitalInput( ) (_TRISA8 = 1)
Configures the RA8 GPIO Pin which has a custom name of IO_RA8 as Input.
| none |
none |
IO_RA8_SetDigitalOutput
#define IO_RA8_SetDigitalOutput( ) (_TRISA8 = 0)
Configures the RA8 GPIO Pin which has a custom name of IO_RA8 as Output.
| none |
none |
IO_RA8_SetHigh
#define IO_RA8_SetHigh( ) (_LATA8 = 1)
Sets the RA8 GPIO Pin which has a custom name of IO_RA8 to High.
The RA8 must be set as Output Pin |
| none |
none |
IO_RA8_SetLow
#define IO_RA8_SetLow( ) (_LATA8 = 0)
Sets the RA8 GPIO Pin which has a custom name of IO_RA8 to Low.
The RA8 must be set as Output Pin |
| none |
none |
IO_RA8_Toggle
#define IO_RA8_Toggle( ) (_LATA8 ^= 1)
Toggles the RA8 GPIO Pin which has a custom name of IO_RA8.
The RA8 must be set as Output Pin |
| none |
none |
Function Documentation
PINS_Initialize()
void PINS_Initialize (void )
Initializes the PINS module.
| none |
none |
3.29.5.2 File Documentation
3.29.5.2.1 source/pins.h File Reference
#include <xc.h>
Functions
void PINS_Initialize (void)
Initializes the PINS module.
Macros
#define IO_RA5_SetHigh() (_LATA5 = 1)
Sets the RA5 GPIO Pin which has a custom name of IO_RA5 to High.
#define IO_RA5_SetLow() (_LATA5 = 0)
Sets the RA5 GPIO Pin which has a custom name of IO_RA5 to Low.
#define IO_RA5_Toggle() (_LATA5 ^= 1)
Toggles the RA5 GPIO Pin which has a custom name of IO_RA5.
#define IO_RA5_GetValue() _RA5
Reads the value of the RA5 GPIO Pin which has a custom name of IO_RA5.
#define IO_RA5_SetDigitalInput() (_TRISA5 = 1)
Configures the RA5 GPIO Pin which has a custom name of IO_RA5 as Input.
#define IO_RA5_SetDigitalOutput() (_TRISA5 = 0)
Configures the RA5 GPIO Pin which has a custom name of IO_RA5 as Output.
#define IO_RA8_SetHigh() (_LATA8 = 1)
Sets the RA8 GPIO Pin which has a custom name of IO_RA8 to High.
#define IO_RA8_SetLow() (_LATA8 = 0)
Sets the RA8 GPIO Pin which has a custom name of IO_RA8 to Low.
#define IO_RA8_Toggle() (_LATA8 ^= 1)
Toggles the RA8 GPIO Pin which has a custom name of IO_RA8.
#define IO_RA8_GetValue() _RA8
Reads the value of the RA8 GPIO Pin which has a custom name of IO_RA8.
#define IO_RA8_SetDigitalInput() (_TRISA8 = 1)
Configures the RA8 GPIO Pin which has a custom name of IO_RA8 as Input.
#define IO_RA8_SetDigitalOutput() (_TRISA8 = 0)
Configures the RA8 GPIO Pin which has a custom name of IO_RA8 as Output.
#define IO_RA11_SetHigh() (_LATA11 = 1)
Sets the RA11 GPIO Pin which has a custom name of IO_RA11 to High.
#define IO_RA11_SetLow() (_LATA11 = 0)
Sets the RA11 GPIO Pin which has a custom name of IO_RA11 to Low.
#define IO_RA11_Toggle() (_LATA11 ^= 1)
Toggles the RA11 GPIO Pin which has a custom name of IO_RA11.
#define IO_RA11_GetValue() _RA11
Reads the value of the RA11 GPIO Pin which has a custom name of IO_RA11.
#define IO_RA11_SetDigitalInput() (_TRISA11 = 1)
Configures the RA11 GPIO Pin which has a custom name of IO_RA11 as Input.
#define IO_RA11_SetDigitalOutput() (_TRISA11 = 0)
Configures the RA11 GPIO Pin which has a custom name of IO_RA11 as Output.
Detailed Description
PINS Generated Driver Header File