5.6 Set BT TX Power
The following table describes how to set the BT TX power command structure. This command is used to set the transmit power to a specific level.
| HCI Packet Indicator | Op Code | Parameters Length | Parameters Payload | |
|---|---|---|---|---|
| 1 | 0xFC3B | 3 | Reserved (2 bytes) | TX Level (1 Byte) |
The TX levels can be set to one of the following values, 0, 3, 6, 9, 12, 15, 18. Values other than those recommended will be floored to the nearest supported level. A maximum level might be enforced by the firmware to comply to RF regulations.