5.4 Vendor-Specific Reset
The following table describes the vendor-specific Reset. This command is used when the Boot ROM is running on the host controller only. It is issued after new firmware is downloaded to the Bluetooth controller's memory to start the command.
| HCI Packet Indicator | Op Code | Parameters Length | Parameters Payload |
|---|---|---|---|
| 1 | 0xFC55 | 0 | N/A |