7 Appendix 1: Programming the Device Using FlashPro Express
(Ask a Question)This section describes how to program the PolarFire device with the Job
programming file using a FlashPro programmer. The default location of the Job file is
located at the following location:
mpf_an4950_v2023p1_df\Programming_Job\top.job
To program the PolarFire device using FlashPro Express, perform the
following steps:
- Ensure that the jumper settings on
the board are the same as listed in Table 5-2.Important: The power supply switch must be switched off while making the jumper connections.
- Connect the power supply cable to the J9 connector on the board.
- Connect the USB cable from the Host PC to the J5 (FTDI port) on the board.
- Power on the board using the SW3 slide switch.
- On the host PC, launch the FlashPro Express software.
- To create a new job, click
New or in the Project menu, click
New Job Project from FlashPro Express Job as shown in the
following figure.
Figure 7-1. FlashPro Express Job Project - Enter the following files in the
Create New Job Project dialog box:
- Programming job
file: Click Browse, navigate to the
location where the
.jobfile is located, and select the file. The default location is:mpf_an4950_v2023p1_df\Programming_Job\top.job. - FlashPro Express job project location: Click Browse and navigate to the location where you want to save the project.
Figure 7-2. New Job Project from FlashPro Express Job - Programming job
file: Click Browse, navigate to the
location where the
- Click OK. The required programming file is selected and ready to be programmed in the device.
- The FlashPro
Express window appears as shown in the following figure. Confirm that
a programmer number appears in the Programmer field. If it
does not, confirm the board connections and click Refresh/Rescan
Programmers.
Figure 7-3. Programming the Device - Click RUN.
When the device is programmed successfully, a RUN PASSED
status is displayed as shown in the following figure.
Figure 7-4. FlashPro Express—RUN PASSED - To close FlashPro Express, click the close button or on the Project tab, click Exit.