8 Appendix 2: Running the Tcl Script
(Ask a Question)TCL scripts are provided in the design files folder under directory TCL_Scripts. If required, the design flow is reproduced from Design Implementation till generation of job file.
To run the TCL, perform the following steps:
- Launch the Libero software.
- Click .
- Click Browse and
in the downloaded
TCL_Scriptsdirectory, selectscript.tcl. - Click Run.
After successful execution of TCL script, Libero project is created within TCL_Scripts directory.
For more information about TCL scripts, see
mpf_an4950_v2023p1_df\TCL_Scripts\readme.txt
For more details on TCL commands, see Tcl Commands Reference Guide .