6.3 Info Command
The
Info command accesses some static or dynamic status
information from the device depending upon the parameters input to the command. The specific command modes include:- Revision
- Returns a value indicating the device identification byte and the revision number of the device. It is recommended that software not depend on the revision information as it may change over time.
- LockStatus
- Returns a value
indicating if the Slot selected in either the Configuration or Data zone is
locked or unlocked. After the
Deletecommand has been run this mode will always fail. - ChipStatus
- Returns a value. The first byte returned indicates if the Delete command has been used to clear the data slots.