10 Soldering Recommendations
The BM83 module can be soldered to the host board using standard leaded and lead-free solder reflow profiles. The BM83 module is assembled using a standard lead-free reflow profile, IPC/JEDEC J-STD-020.
To avoid the damage to the module, it is mandatory to follow the recommendations as listed:
- Refer to AN233 Solder Reflow Recommendation Application Note for the soldering reflow recommendations.
- Do not exceed peak temperature (TP) of +260ºC.
- Use no-clean flux solder paste.
- Do not wash the module as moisture can be trapped under the shield.
- Use only one flow. If the PCB requires multiple flows, apply the module on the final flow.
The following figure illustrates the reflow profile of the BM83 module.