4.3 Programming the Device
(Ask a Question)This section describes the steps to program the PolarFire SoC device with the
VKPFSoC_H264.job file using FlashPro Express.
Follow these steps:
- Ensure to close pins 1 and 2 of J28 jumper.
- Connect a micro-USB to J5 from the host PC and start the FPExpress software from .
- Ensure to power on the PolarFire SoC video kit.
- Select New or
New Job Project from the Project menu to create a
new job project, see the following figure.
Figure 4-3. New FlashPro Express Project - In the New Job Project
dialog box, enter the following:
- Programming job file: Click Browse and navigate to the location where the job file is located and select the file.
- FlashPro Express job project location: Select Browse and navigate to the location where you want to save the project.
- Click Open. The required programming file is selected and ready to be programmed in the device. The FlashPro Express window appears. Confirm that a programmer number appears in the Programmer field. If it does not, check the board connections and click Refresh/Rescan Programmers.
- Click RUN to program the device. When the device is programmed successfully, a RUN PASSED status is displayed.
- Close FlashPro Express (Project > Exit).
- Power-cycle the board.