4.2 Setting Up the Serial Terminal
(Ask a Question)PolarFire SoC Video kit includes CP2108 USB to UART chip to interact with on-board Linux OS.
Before you start:
- Download and install CP210x Universal Windows Driver.
- Unzip and see the CP210x_Universal_Windows_Driver_ReleaseNotes.
After installing the driver, follow these steps:
- Connect USB cable at J12 port on the PolarFire SoC video kit board to the host PC.
- After connecting the power adapter to the board
at J39, switch ON the boards power supply using the SW5 switch. This must
detect the USB UART chip on the board at the host PC. You can confirm this at the
host PC device manager, see the following figure.
Figure 4-1. Device Manager The interfaces on the host PC's device manager are active in the current demo project and display the messages when appropriately configured.
Interface 0 displays the Hart Software Service (HSS) boot messages while Interface 1 displays U-Boot messages, Linux boot messages, and provides a Linux prompt.Important: For each user, the interfaces might be on a different COM# than what is shown in the preceding figure.An application like MobaXterm/TeraTerm at the host PC is required to establish serial communication with the video kit board. The baud rate for such connections must be 115200 bps, see the following figure.Figure 4-2. Serial Port Settings - Open Interface 0 and Interface 1.
Important: The data rate must be configured for all interfaces to
establish successful communication with the PolarFire SoC video kit.