5.1 Flashing Linux .wic Image in eMMC Mode
(Ask a Question)This section describes the steps to put the HSS in CLI mode, program the Linux images into eMMC using the USBImager application and initiate the Linux boot.
- Do not insert SD card to the board. If present, SD card booting takes priority.
- Remove the micro-USB cable connected to J5 and connect it to J19 (USB-OTG connector) of the board. When the USB cable is detected, the LED near J19 glows in green.
- Connect one more micro-USB cable to J12 from the host PC.
- J18 and J57 must be open.
- Close pins 2 and 3 of J36.
- Power ON the board and press Enter on Interface 0
while booting.Important: The COM port number might be different for different users. To identify the COM port, see Setting Up the Serial Terminal.
- Follow the steps in eMMC Content Update Procedure.
- After programming the eMMC and
rebooting, check the serial terminal application connected to Interface 1. Linux
will be up and running, waiting for user to login.
Figure 5-1. Linux User Login
This step demonstrated the process of running the Linux user application by programming
the Linux user application image onto the on-board 8 GB eMMC NAND Flash using the
.wic file. Upon completion, the Linux OS booted up successfully
from the eMMC as indicated by the Linux OS login prompt displayed to the user.